STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500

Hello,i am trying to configure the STUSB4500 on a Eval-SCs001v1 with a F446RE Nucleo board using I2C connection. from my understanding am i unable to use the GUI to make the NVM files because that wont reconize my Nucleo board. Also the example proje...

ThomasDisSensors_0-1718193967638.png ThomasDisSensors_1-1718196101906.png

Resolved! STM32H7 ADC DMA don't run with LWIP and RTOS

Hello everyone,I have to use the ADC 16b converter with DMA which does not work if DCache is enabled but, to use LWIP and RTOS it is necessary that DCache is enabled.Does anyone know how to fix the problem?Thank you in advance

Stefano1 by Associate II
  • 2105 Views
  • 2 replies
  • 0 kudos

Overwrite 4 Bytes at given location in Hex file

Write 4 Bytes at given location in Hex file (Flash segment)I tried this:const uint32_t __attribute__ ((section(".checksumdata"), used)) CodeChecksum = 0x12345678; But when I build code, It doesn't changes only ".checksumdata", but also other intermit...

Jayant_0-1715865618048.png Jayant_1-1715865693572.png
Jayant by Associate II
  • 4028 Views
  • 7 replies
  • 3 kudos

stm32 UART Hardware Flow RTS/CTS

Posted on March 05, 2014 at 09:06Hello, Im Trying to Communicate between Stm32 to FT5000(Lon ShortStack) through UART Hardware Flow ,...I need to Assert and De-assert RTS/CTS,.....How do i achieve this ,....? Please Help,Thank You,Sanil  #stm32-u...

sundar by Associate II
  • 7328 Views
  • 6 replies
  • 0 kudos

Resolved! STM32H745 with WIFI

Hello,I plan to use STM32H745 controller with touchGFX for UI. Additionally need WIFI capability. What options are available if WIFI is to be used with STM32H745? I dont want to invest time in developing a communication protocol to communicate with a...

ATank.1 by Associate III
  • 2175 Views
  • 2 replies
  • 0 kudos

HAL_Delay() crashes STM32 code

I'm trying to upload code to an STM32F103RET6 MCU and have a simple setup by now (see image below). I have attached a LED to pin PA1 as a GPIO OUTPUT and an external oscillator at 16 MHz. The other three pins are connected to the JTAG connector that ...

0693W00000ANu5wQAD.png 0693W00000ANu6BQAT.png 0693W00000ANu6fQAD.png
AReye.1 by Associate II
  • 10095 Views
  • 10 replies
  • 0 kudos

Resolved! CAN bus stop working when cpu is put in sleep (STM32F205VGTX)

On STM32F205VGTX, when I put cpu in sleep by using this command: HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI); CAN peripheral stops working. It does not acknowlege bus messages anymore and there is no CAN interrupts to wake up...

HSagh.1 by Associate II
  • 2133 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.