STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding stm32h750 USART IDLE

Hello,     BIT4 IDLE Bit of USART interrupt and status register (USART_ISR)             Could you please explain what is  condition about  "an idle Line is detected"?        How long time for the  UART RX Pin on idle state?         the idle is high l...

q4.png
martin_xu by Associate II
  • 1526 Views
  • 1 replies
  • 0 kudos

Default struct fields alignment

Hello,which is the default struct fields alignment policy of GCC, on STM32 MCU? I have the following structure: typedef struct{  uint32_t   param1;  float      param2;  uint16_t   param3;} PARAM_T;  I expected a size of 10 bytes, but it is 12 instead...

CTabo.1 by Senior
  • 2564 Views
  • 2 replies
  • 0 kudos

OSPI in QSPI mode, issue with sending address

I'm importing some QSPI code we've been using a few years from an SMT32F7xx project to a new project using an STM32L4xx. Both projects use the same target device. I'm having an issue where the majority of messages don't seem to be sent. After debuggi...

TimJones by Associate
  • 5219 Views
  • 8 replies
  • 3 kudos

Resolved! I can't connect my Nucleo to my STM32L0 board

Well, I'm new to the STM32. I'm developing vibration and temperature sensors, which used to be equipped with an atmega.With the new demand for processing I decided to upgrade by putting an STM32L0 in place of the old controller.The problem is that no...

Resolved! CAN initializing issue

Hi ST-CommunityI am working on CAN Communication in F103When I am de-initializing properly , But when , I am reinitializing it is not workingPlease tell me how to reinitialize CAN Communication if (0 == HAL_GPIO_ReadPin(BRAKE_GPIO_Port, BRAKE_Pin)) {...

Resolved! Zephyr: how DAC on STM32H723ZG ?

Dear all,does anyone have experience with setting analog output signals via Zephyr RTOS? I managed to get the D/A conversion on the Nucleo H723ZG to run via STM32CubeIDE, but I’m running intro trouble when using Zephyr. Apparently a "DAC" driver is r...

Lysandros by Associate II
  • 4127 Views
  • 4 replies
  • 2 kudos

Update firmware from W25Qxx flash

I use a board with STM32F405 + W25Qxx. At the moment, I have implemented downloading the firmware file to an external flash memory (via CAN). The process of downloading and verification is implemented in the main firmware. It is necessary to implemen...

Kuzma30 by Associate II
  • 2417 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.