2024-06-23 5:09 PM
Well, I'm new to the STM32. I'm developing vibration and temperature sensors, which used to be equipped with an atmega.
With the new demand for processing I decided to upgrade by putting an STM32L0 in place of the old controller.
The problem is that now I can't use my CUBE Programmer to connect to my board via Nucleo's STM Link.
An error message appears whenever I click Connect, and my Nucleo board flashes red.
I think I may have made a connection or PCB design error.
Information:
My system has 1 accelerometer 1 temperature sensor 1 Lora radio 1 battery sensor and a 3v3 regulator.
The clock has been set to 25KHz by means of an Oscillator Crystal.
and the BOOT0 pin is not connected to anything other than the pull-down resistor.
Solved! Go to Solution.
2024-06-24 12:03 PM
Ok, so now it sees the ST-LINK
The complaint is the target is not viable.
So power and connections become critical. Schematic looks reasonable. Check components and orientation. Common grounds. Check state/level of NRST signal
The target will need both analogue and digital supplies connected.
SWCLK, SWDIO, GND
The CM0(+) will not support PB3/SWO
Disconnect the local target on the NUCLEO-F103RB board, pair of jumpers.
2024-06-23 7:25 PM - edited 2024-06-24 11:57 AM
The error is that it can't even find the ST-LINK / NUCLEO, so perhaps a short or power issue.
I'd assume you've used the NUCLEO previously? Which model of NUCLEO?
Does it show up in Device Manager?
2024-06-24 5:19 AM
2024-06-24 11:10 AM
@MatheusMarkies wrote:I made a new board soldering only the STM32 system and now my NUCLEO is showing up in the device manager and also in the Programmer.
However, I can't connect to it.
So you're using the ST-Link part of your Nucleo board to program your own custom board?
Are you sure you've set all the links correctly for that?
Does the Nucleo's ST-Link still work with the Nucleo Target?
2024-06-24 12:03 PM
Ok, so now it sees the ST-LINK
The complaint is the target is not viable.
So power and connections become critical. Schematic looks reasonable. Check components and orientation. Common grounds. Check state/level of NRST signal
The target will need both analogue and digital supplies connected.
SWCLK, SWDIO, GND
The CM0(+) will not support PB3/SWO
Disconnect the local target on the NUCLEO-F103RB board, pair of jumpers.
2024-06-25 4:43 AM
2024-06-25 5:03 AM
@MatheusMarkies wrote:I won't have SWO support on this chip, so I'm not sure how I can debug it
You don't need SWO to debug - only SWCLK & SWDIO.
Use a UART TX out to give "realtime" diagnostic output ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.