2024-06-16 11:27 PM
Dear all,
does anyone have experience with setting analog output signals via Zephyr RTOS? I managed to get the D/A conversion on the Nucleo H723ZG to run via STM32CubeIDE, but I’m running intro trouble when using Zephyr. Apparently a "DAC" driver is required, however the documentation is not very clear.
Thanks
Solved! Go to Solution.
2024-06-25 3:40 AM
Hello Lysandros,
Sorry for the confusion! the STM32H723 is supported: Zephyr supported boards
zephyr/boards/arm/: This directory contains board configuration files for ARM architecture-based boards such as V2M, MPS2, and MPS3, which are ARM Versatile Express boards.
zephyr/boards/st/: This directory is specifically for ST boards. The naming convention here is more vendor-specific, focusing on ST's product lines like the Nucleo series, which includes models such as H743ZI and H723ZG.
"No SOURCES given to Zephyr library: drivers__dac": this could happen if the CMakeLists.txt file for the DAC driver is missing the necessary source files
Regarding trainings, this is all I can think about:
GitHub - zephyrproject-rtos/hal_stm32
https://docs.zephyrproject.org/latest/
https://discord.com/invite/Ck7jw53nU2
You can check PR issues here: https://github.com/zephyrproject-rtos/zephyr/labels/platform%3A%20STM32
Use STM32Cube in your application: https://github.com/zephyrproject-rtos/hal_stm32#use-stm32cube-in-your-application
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-17 12:59 AM
Hi,
>running intro trouble when using Zephyr
Why ? Using RTOS or not - you just write to the DAC , no "driver" needed.
When using Cube/HAL , to setup the chip configuration, just use the HAL functions or write direct to DAC .
2024-06-20 10:25 AM
Hello @Lysandros,
You can use STM32H743 as a reference as the Nucleo H723ZG is not yet supported in Zephyr.
You'll need to create a new board definition under zephyr/boards/arm/, in which you add the board config (board.dts, board_defconfig, Kconfig.board , andCMakeLists.txt)
There is already a sample of DAC with STM32H743.overlay here
This is not a simple task, but it is worth it if you're willing to invest some time learning the whole Zephyr architecture
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-23 2:23 AM - edited 2024-06-23 2:24 AM
Hello @Sarra.S ,
thanks for your reply and this hyperlink.
I have a few follow-up questions:
Best regards
Lysandros
2024-06-25 3:40 AM
Hello Lysandros,
Sorry for the confusion! the STM32H723 is supported: Zephyr supported boards
zephyr/boards/arm/: This directory contains board configuration files for ARM architecture-based boards such as V2M, MPS2, and MPS3, which are ARM Versatile Express boards.
zephyr/boards/st/: This directory is specifically for ST boards. The naming convention here is more vendor-specific, focusing on ST's product lines like the Nucleo series, which includes models such as H743ZI and H723ZG.
"No SOURCES given to Zephyr library: drivers__dac": this could happen if the CMakeLists.txt file for the DAC driver is missing the necessary source files
Regarding trainings, this is all I can think about:
GitHub - zephyrproject-rtos/hal_stm32
https://docs.zephyrproject.org/latest/
https://discord.com/invite/Ck7jw53nU2
You can check PR issues here: https://github.com/zephyrproject-rtos/zephyr/labels/platform%3A%20STM32
Use STM32Cube in your application: https://github.com/zephyrproject-rtos/hal_stm32#use-stm32cube-in-your-application
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.