STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FMC memory in fmc display

hello, I have a display configured for FMC but I would like to add a framebuffer to the RAM memory, unfortunately the MCU memory is not enough (the display resolution is 480x800) so I have to add external RAM. My question is how to do it since I am a...

how to program the option bytes within firmware

Hello,After reading the following threads:How to program STM32 Option Bytes with the HAL API - STMicroelectronics CommunityWhat are option bytes in STM32 and how do I use th... - STMicroelectronics CommunityProblem with option bytes set from program ...

KoSt by Associate III
  • 1116 Views
  • 0 replies
  • 0 kudos

USB type C not working.

I have made my own PCB with STM32F427VIT6 for a project. But if I tried connecting with the cube IDE, I could not connect it through the Type C port, I could only connect it with STlink. Even my laptop doesn't detect the port. Can anyone help debug t...

Jeeva_0-1719565471971.png Jeeva_1-1719565698288.jpeg
Jeeva by Associate II
  • 3781 Views
  • 6 replies
  • 1 kudos

Resolved! External oscillator issue ( stm not booting)

Hello, I have designed my PCB with stm32f427VIT6 and a 24Mhz crystal oscillator. I was trying to upload and test the normal blink code and it's not working. If I disable the external clock, the LED works and does not work with an external clock. I am...

Jeeva_0-1719489952248.png Jeeva_1-1719489972408.png Jeeva_2-1719490012982.png
Jeeva by Associate II
  • 5021 Views
  • 8 replies
  • 8 kudos

Resolved! Effect of live wire insertion/removal of SPI signals

Hello, I am looking for a solution to my problem.I am using an STM32C031 to light LEDs using SPI signals.I am using a connector to connect the STM32 mounting board to the LED mounting board. The connector connects the DC power supply and the SPI sign...

shank by Associate III
  • 3064 Views
  • 6 replies
  • 0 kudos

Resolved! Add External SRAM to STM32H743 without FMC

Hello,I am trying to find available solutions for below requirement.I am using STM32H743 MCU in a design and I want to add external SRAM of 128Mbytes to the design.I understand can do this with FMC, but the problem is available pins for the FMC are c...

Blk81 by Associate II
  • 6702 Views
  • 9 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.