STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to choose crystal speed?

I just was wondering how you guys proceed to choose an external crystal, specifically what speed it should have...The clock management with its tons of PLLs and dividers seems to be able to scale up almost any source to a desired frequency.for the L4...

b.a. by Associate III
  • 11727 Views
  • 16 replies
  • 2 kudos

Selecting GPIO in shared pins for STM32G030F6

In pins that share more than one GPIO, how do you set the GPIO to connect to the physical pin?For instance, for pins PA12/PA10 and PA11/PA9 one can remap them using SYSCFG_CFGR1 register. But is unclear for the rest of the pins. For example, TSSOP20 ...

How to set Adc for maximum rate

I have design  pcb for Stm32H723VGT6 ( 100 pins  TQFP )  my job is read adc 12 bit and transfer over usb to PC  . i have set sysclk to 550 MHz and ADC clock to 64 MHz  so i got sample rate to 1.3 Msps but mcu are hot. So i have sysclk to 400 and ADC ...

tawat25 by Associate
  • 1235 Views
  • 1 replies
  • 0 kudos

Resolved! STSPIN32G4 and PC13-PC14-PC15 for LED Indicators

Good morning,In regards to the current limit placed on the PC13-PC15 pins of the STM32G431VBx3 that is used as the basis of the STSPIN32G4 (and whose datasheet is referred to multiple times in the STSPIN's), the '431 datasheet has the usual low-power...

MLange_0-1719568668520.png
MLange by Associate
  • 1804 Views
  • 1 replies
  • 2 kudos

Resolved! STM32F407 MCU Maximum Voltage Input

Hi AllMaximum input voltage for this series of MCU per Table II of the datasheet is specified to be 4.0 VDC for all pins other than five-volt tolerant. Table 12 specifies the maximum injected current for all pins other than five-volt tolerant to be +...

IKhan.2 by Associate II
  • 4906 Views
  • 5 replies
  • 1 kudos

Resolved! Problem with UART interrupt

Hi,I have two MCU communicating with each other via RS485. It's a very simple code one MCU send a data to other and the other is trying to receive this. With MCU2 code everything is fine. It sends data like it should be.Problem is with MCU1 code. Whe...

Raf_al by Associate III
  • 6177 Views
  • 13 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.