STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STANDBY and SLEEP Modes using RTC

Hello,I am trying to use the SLEEP and STANDBY modes with the RTC. I want the device to go to sleep/standby mode for 10 seconds and wake up after the 10 seconds are done. I have tried it with an interrupt using UART and Button and both the modes are ...

Resolved! From H7-series to U5-series - problem with OCTOSPI

Hi,I have two custom boards using the same OCTOSPI HyperFlash and for some reason the memory fails to run at higher speeds with U5-board.Board 1-H7 MCU at 550 MHz-OCTOSPI at 160 MHz works fine! (max clk is 166 MHz)Board 2-H5 MCU at 160 MHz-OCTOSPI at...

Resolved! APB1 and APB2 are out of sync

I'm using STM32F446.I'm generating PWM signals using TIM1 and TIM8 (on APB2, which runs at 90MHz, and 180MHz for the timers).I'm also generating PWM signals using TIM4 and TIM12 (on APB1, which runs at 45MHz, and 90MHz for the timers).I start each PW...

SZano by Associate III
  • 4692 Views
  • 8 replies
  • 2 kudos

Resolved! Communication between STM32C011 and EEPROM M24C0

Chào bạn,Tôi đã thiết lập kết nối theo sơ đồ và tôi đã tải mã trong tệp đính kèm nhưng tôi không thể đọc dữ liệu từ EEPROM. Địa chỉ M24C02 của tôi được đặt thành 0xA0.Ai đó có thể giúp tôi xác định vấn đề? Cảm ơn rất nhiều.  

HauDO_1-1718248224550.png
HauDO by Associate II
  • 7149 Views
  • 10 replies
  • 2 kudos

Resolved! VBus triggered by Data pins STM32H743?

I have a board that uses the H743 and have been having major problems with the USB side of things. I've only just realised that I left VBus floating all this time, so I'm assuming that's a major cause of my issues.. The board I have is designed as a ...

Resolved! External RAM for FrameBuffer on STM32H7S7L8

Good morning to all,I’d like to ask your advice.I have to insert an external RAM for the framebuffer because the internal one is not enough for LCD that I will drive (LCD-TFT LVDS 7 inch 1024x600).Which external RAM do you recommend? Could a QuadSPI ...

Leo99 by Associate III
  • 3730 Views
  • 6 replies
  • 1 kudos

Resolved! Error: No STM32 Target Found - But only in CubeProgrammer

Hello, I've been using the Nucleo-F446RE to program a stm32f4 series chip using the Nucleo's onboard ST-link capabiltiies. So far I have managed to get it to link and work in CubeIDE, but in CubeProgrammer it's giving me the following issue (attached...

raridi_0-1719501344798.png
raridi by Associate
  • 1490 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.