STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750VBT6 DCMI USART

With DCMI (with DMA) and USART only 1.5FPS, why is the frame rate really low? The output is set to QVGA and formatted as JPEG.  

Shiina_0-1720607635646.png Shiina_1-1720607659868.png Shiina_2-1720607674883.png
Shiina by Associate III
  • 3725 Views
  • 8 replies
  • 0 kudos

Resolved! STM32G4 flash banks description ambiguity

Hello,I'm currently designing a bootloader and an application for stm32g474ccu6 MCU (256kB flash). Today I wanted to implement a bootloader feature allowing the user app to take up more than one flash bank in flash memory (Im working in dual bank mod...

Resolved! HAL_CAN_Transmit behavior for CAN Bus OFF

Hi,When i use HAL_CAN_Transmit to send a CAN message on STM32F4, if say I am in error passive or bus off condition, what error does the API return? If I am in error passive, what is the best way to reset the error count to 0?Where can i get the error...

krishr by Associate III
  • 3723 Views
  • 4 replies
  • 0 kudos

Baud rate

In a spectroscopy application I am sampling the incoming values at 300kHz with a 12-bit ADC so i will be having a bit rate of 3.6Mbps do i need to have the same baud rate. I am doing it using stm32f401re

000harsha by Associate II
  • 1848 Views
  • 3 replies
  • 0 kudos

Suitble Hyperram for STM32H735

HiI'm designing a PCB using the STM32H735 based on the eval kit STM32H735G-DK.Since the HyperRAM  S70KL1281 on the eval is EOL I'm looking for an alternativeI have read a few posts with issues on this subject and I'm usure which part i should go with...

Kvang by Associate III
  • 2125 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.