STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADE9000 COMMUNICATION PROBLEM WITH STM32F401

I have setup a base board of ADE9000 With only Basic Components connected, Like Bypass capacitors, Reset pullups and connected SPI Directly with the STM32F401 Blackpill board , Everything starts-up perfectly.So I want to check the communication betwe...

Caan by Senior
  • 4049 Views
  • 5 replies
  • 2 kudos

Resolved! stm32f746 ETHERNET issue

Hi, Could anyone help with this problem? Its driving me mad!!! I have designed an ethernet interface  for an F746-100 MCU I have changed pins to avoid using Port G and I have used the  circuit below. The RJ45 connector is a standard RB1-125BAG1A and ...

STM32F4 Possible to disable CAN bootloader?

I have a product that contains 2 STM32F405/07/15/17 series MCUs. There are 2 because we need 4 CAN and that's cheaper and easier than finding a 4 CAN MCU. Anyways, the main MCU is connected to the secondary MCU via UART and the boot/reset pins so tha...

LLawr.1 by Associate II
  • 1647 Views
  • 2 replies
  • 0 kudos

STM32H7 ECC IRQ

I am trying to understand how the ECC IRQs work.  I have configure the RAMECC1 AXI SRAM, RAMECC2 SRAM1, 2 and 3, and RAMECC3 SRAM 4 monitor CR registers to generate interrupts on double bit errors.  I have configured the IER so that Global interrupts...

NBrick67 by Associate II
  • 1196 Views
  • 1 replies
  • 0 kudos

Resolved! ISR function timing period issue

Hi        We are working on STM32H503 MCU which has ARM Cortex 33. In datasheet it is provided that 12 cycles or instruction to enter into an interrupt function. Configured system clock as 250MHz, with that we could reach an interrupt function within...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.