STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FT812, Correct way to manually configure SPI?

Hi guys, I'm fairly a newbie to stm32 so please forgive me if I make some mistakes, I'm trying to configure a driver code for a SPI FT812 NHD display on STM32G474VETx chipset, so far I've been able find a driver code and ported it over onto STM32, ho...

Resolved! Short read from multiple ADCs under DMA

Using a stm32f303RE Nucleo board which has 4 (independent ?) ADC blocks.I'm trying to read a single channel from each of the 4 ADC under DMA simultaneously triggered from the same timer update event but I'm only getting about 30-40% of the data I'm a...

Resolved! STM32G491RE MCU getting struck

Hi,I am working on stm32g491re custom board.I am using STM32cubeide  and segger jlink debugger with serial wire debug.After flashing the firmware program getting struct at intializationlike HAL_GPIO_INIT()and HAL_TIMER_init()if I try to suspend the r...

STM32H725 temperature sensors

Hello, I am trying to measure Junction temperature of the STM32H725IG device.ADC3 is configured as an errata say to have only temperature channel 17 and continuous measurement. Temperature I see seems to be between 60 and 80 degree Celsius.I tried al...

Resolved! PWM on STM32U599

Dear All,I am attempting to migrate a project from a STM32F74NGH MCU to a STM32U599NJH MCU.In the F7 MCU I am applying the PWM on CH1 of TIM3 that corresponds to pin PB4.On the new setup I need to apply the PWM to pin PC5, which corresponds to TIM1, ...

G_Anastasopoulos_0-1722607604849.png G_Anastasopoulos_1-1722607624978.png G_Anastasopoulos_2-1722608382008.png G_Anastasopoulos_3-1722608787175.png

Resolved! Modification/Clarification of Chirp Signal Code

Hello, first of all, I hope im at the right section for my question. If not I'm sorry.I'm relativ new in working with Nucleo Boards and currently working on a Project where i want to generate a chirp signal/sinus sweep from -20kHz up to 20kHz.I made ...

Screenshot 2024-08-01 133717.png Screenshot 2024-08-01 133819.png

Resolved! LwIP integration with external PHY

Hello, is it possible to ușe the LwIP Middleware over the low level library for an external PHY such as ENC28J60?If so, could you pinpoint me to a documentation or an article?Thanks.

TheoMj by Associate
  • 2721 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.