2024-08-02 5:58 AM - edited 2024-08-02 5:59 AM
Hi,
I am working on stm32g491re custom board.
I am using STM32cubeide and segger jlink debugger with serial wire debug.
After flashing the firmware program getting struct at intialization
like HAL_GPIO_INIT()
and HAL_TIMER_init()
if I try to suspend the running/restart the controller through IDE i am getting issue like below
No source available for "(gdb[18].proc[42000].threadGroup[i1],gdb[18].proc[42000].OSthread[1]).thread[1].frame[0]"
and
Break at address "0x1fff469a" with no debug information available, or outside of program code.
Break at address "0x1fff408e" with no debug information available, or outside of program code
In GPIO i am using one exti gpio if i comment it's executing remaining program.
Same happens with timer interrupt also.
Is there thing missing for interrupts and its not happening every time 8 out of 10 times its happening. Any one can suggest
Thanks
Solved! Go to Solution.
2024-08-02 6:05 AM
Looks like it's in the bootloader. Is BOOT0 tied low?
2024-08-02 6:05 AM
Looks like it's in the bootloader. Is BOOT0 tied low?
2024-08-02 6:08 AM
2024-08-02 6:24 AM
Do you set SCB->VTOR to the correct vector table address in flash?
2024-08-02 6:30 AM
@TDK ,@I didn't changed anything in the flash programing.where do I need to check this correct vector address of my mcu is it it datasheet? and where do I need to set this vector address is it is the flash.c ??
Thanks
2024-08-02 6:34 AM
Generally, ensure the USER_VECT_TAB_ADDRESS define is uncommented in system_*.c file.
When you are debugging, you can check the value of SCB->VTOR to ensure it is correct. It should point to 0x08000000.
2024-08-02 8:42 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2024-08-02 9:20 AM
Struck with what? Lightening?
If it's going into ROM you need to check BOOT0 and the content of the words written at 0x08000000, invalid content will cause it to ignore FLASH content
Use STM32 Cube Programmer and show us a dump of the memory block at 0x08000000 should be the stuff read in by default.
Attach Screen Shot, Attach .HEX file
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.