STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446VET7 DMA Transmission

Hello, I am trying to transmit 64 byte data with DMA but if I am not use at least 10ms delay the data is not transmitted. How can I check the is data transmitted without any need of delay ? I try to check UART is busy or not fort that but its not wor...

testbenchmark_0-1724134724919.png testbenchmark_1-1724134740099.png

Resolved! stm32cubeide bug with code generation

I have found an issue with code generation from .ioc file. Using STM32H7S78 DK when choosing pins for FDCAN2 (I chose pb5 and pb6), after code generation it doesnt set pb 6 as an RX. Even if you manualy add it in the code it will remove it after code...

PPopo.1 by Senior
  • 2057 Views
  • 4 replies
  • 0 kudos

Resolved! Nucleo STM32H723ZG - CAN not working

Hello, i have a question about the stm32h723. I tried setting up the CAN peripheral and it's not working. I absolutely don't know why. Can anybody help me out please? My Sourcecode looks like the following:/* USER CODE BEGIN Header */ /** *********...

floppy by Associate II
  • 6731 Views
  • 12 replies
  • 2 kudos

ADC WITH MULTIPLE CHANNELS IN STM32H503

HICan anyone have example how to configure and use multiple ADC channels in STM32503 microcontroller.i have seen in a video to use DMA, but how to configure and use it.anyone please suggest and help.

Singh_t by Associate II
  • 1488 Views
  • 1 replies
  • 0 kudos

Question of STKNX

Regarding the KNX TP, I tested the STKNX evaluation board and my board which have ST-KNX chip then have below questions: Q1, The testing connection is       UART TX => KNX_TX (STKNX EV1) => KNX_TP line => KNX_RX(STKNX chip board 2) => UART RXCH1: KNX...

JFung1_0-1724153013572.jpeg JFung1_1-1724153013575.jpeg JFung1_2-1724153049985.png
JFung.1 by Associate III
  • 1086 Views
  • 0 replies
  • 0 kudos

Resolved! FSMC on STM32F103ZG vs FMC on STM32H755ZI

Good Day and Hello Everyone. In my upcoming project, my task is to upgrade the currently used MCU from STM32F103ZG to STM32H755ZI. My question are;1- Can I replace all the FSMC I/O pins that I'm currently using on STM32F103ZG with the FMC I/O pins on...

mdfsl by Associate II
  • 3372 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.