STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reset after firmware upgrade

Posted on January 23, 2014 at 12:00I have used the STM32 USB-FS-Device development kit examples to implement the custom HID and the DFU. It all works OK and I can upgrade the custom HID application from the DFU application using DfuSeDemo.  The prob...

lee by Associate II
  • 6293 Views
  • 12 replies
  • 0 kudos

Problems with ADC data

Hello,We are uing STM32F303RBT6 controller to read the current parameters of stepper motors.So, 7ADC1 ADC channels are used, which are read through DMA1 Channel1 . InitADC() driver initialization is succesfull, StartADC() conversion is called once ev...

Read data in device sent by host over USB HID

In an STM32CubeIDE USB HID project for an STM32F103C8 board I can send data from the device to the host using the USBD_HID_SendReport() function, like so:USBD_HID_SendReport(&hUsbDeviceFS, (uint8_t*)&hid_report,sizeof(hid_report));How can I read data...

Resolved! stm32h747I-disco sdram cas

 I'm using STM32H747i-DISCO board. In Stm32Cube_FW_H7_V1.11.2 STM32H747I-DISCO example project -- stm32h747i_discovery_sdram.c, cas is 3. SDRAM worked fine with this setting. It didn't work when I changed cas to 2. Datasheet of Is42s32800G-6BLI shows...

GanZ_0-1723473648491.png
GanZ by Associate II
  • 2681 Views
  • 5 replies
  • 0 kudos

Unable to connect STM32F4DISC

Hello thereJust tried connecting my STM32F4DISCOVERY board to my PC. It appears that the underlying operating system recognizes the driver/device correctly. I've tried this on both Windows 10 and Linux and this seems to be the case on both.Here is pa...

Resolved! Reset CM7 Core from CM4 core

Hello. I have a STM32H747XI project. This MCU has both CM4 and CM7 cores. I can reset both of them, when I use NVIC_SystemReset() function. How can I reset only CM7 core from CM4 core?

Gökhan by Associate III
  • 2065 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.