STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bootloader flashing WORD using double WORD

Hi,I want to flash my STM32L452RET6P using a .hex file. I am however struggling with the fact that STM IDE generates a .hex file with lines with only one WORD instead of the only supported double WORD when writing. So I need to buffer and assemble ea...

RBT-ES by Associate III
  • 4347 Views
  • 9 replies
  • 3 kudos

STM32 event system – connection to timers

I have an STM32G473 on an existing board, and now the need to trigger Timer 2 in "One Pulse Mode" from a hardware input has come up. No problem, I thought, as I knew that the MCU has an event system. I simply assumed that I could generate an event wi...

EThom.3 by Senior III
  • 1758 Views
  • 2 replies
  • 2 kudos

Resolved! Error while debug

WHile debugging for a custom board this is what I am facing Break at address "0x1fff4080" with no debug information available, or outside of program code. This is the code that I am trying to run . What is the reason for this error and how it can be ...

Rituraj by Senior
  • 8646 Views
  • 11 replies
  • 2 kudos

Problem getting started with STM32H747I-DISCO

I recently bought a brand new STM32H747I-DISCO board from mouser. Read up user manual and tried to use it for the first time. When I connect it to PC with USB cable, LD10 lights up red. Then LD8 lights up green and LD10 starts blinking red. STM32Cube...

rakib2023 by Associate III
  • 5799 Views
  • 8 replies
  • 0 kudos

STM32H7B0 starting MDMA fails to unexpected IRQ (WWDG)

Dear,We use the STM32H7B0 100 pins version.The MPU, ICACHE, DCACHE are disabledWe will use a MDMA to copy some data from one to another place.Therefore we had try an example to understand the configuration.We had use a part of example:   https://gith...

OGhis by Senior
  • 1937 Views
  • 3 replies
  • 0 kudos

Linker Configuration IAR Setting

Hello,Getting above error if trying to debug and download code in IAR. is there any specific setting required for loader or linker configuration.Controller : STM32H745XI External flash : MTQL512ABB Please find linker details below:  /*###ICF### Secti...

Gajanan_0-1724736990964.png
Gajanan by Associate II
  • 2924 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 Nucleo H7A3ZI board UART Issue

Hi Community, I am facing very basic issue. My UART in H7A3ZI Nucleo 144 board is not displaying correctly on terminal.  My UART Setting:  huart3.Instance = USART3; huart3.Init.BaudRate = 115200; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart...

mahmanish by Associate II
  • 8145 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.