STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI between mcu

@Erwan SZYMANSKI I am trying to establish SPI communication between two STM boards: the Nucleo G431RB as the master and the STM32MP157F-DK2 as the slave. I followed the instructions provided in the Getting Started with SPI guide and configured the se...

nesnes by Associate III
  • 1385 Views
  • 0 replies
  • 0 kudos

Use MOSFETS with STM32 to power up sensors

Hello everyone! I want to use some MOSFETS to individually power up/down sensors on a PCB. Here's the schematics :  The MOSFET is a DMG1012T-7 (N-Channel) and here's it's datasheet : https://www.lcsc.com/datasheet/lcsc_datasheet_1809050424_Diodes-Inc...

yaxsomo_0-1725350654452.png
yaxsomo by Associate III
  • 2182 Views
  • 1 replies
  • 0 kudos

Resolved! CAN Write State issue

Dear, I am trying to run the CAN Communication in STM32F407 discovery board, In CAN_INIT I have made controller state to Ready after that I have changed the controller state from ready to LISTENING in CAN_START function,   but when I am trying to exe...

Resolved! Undocumented behavior of capture/compare registers

Hello,I tried to set a capture/compare register to a value beyond that of the auto-reload register, and the timer I used (TIM8) behaved as if the value had not been written. Reading back gives the expected value though. I haven't dug more but I'm cur...

rbraun by Associate II
  • 1754 Views
  • 6 replies
  • 1 kudos

Resolved! OTG_HPRT>PENCHNG bit in STM32H743

[Not a bug report, explanation below, first post kept for context]I'm writing a USB host library for the STM32H743 rev V. Bits PENA and PENCHNG of register OTG_HPRT represent Port enable and Port enable/disable change. Port enable is supposed to be a...

JBernard_1-1725316374583.png JBernard_2-1725316381451.png lS9ZB1H.png K831E2a.png
JBernard by Associate II
  • 1904 Views
  • 2 replies
  • 1 kudos

Repetition Timer PWM Help

 Hello, I'm wondering if there is an obvious way to generate a limited set of n pulses from an external trigger?At the moment i'm using TIM8 in one pulse mode with repetition but my problem is that i want the White pulse train to start with the risin...

Stemcy_0-1725299151951.png
Stemcy by Associate
  • 2248 Views
  • 4 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.