STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NRST Pin going low while programming for a milli second.

Hii,I am working with stm32f100 series microcontroller, where I am having issue with NRST pin, I have connected a capacitor of 0.1uF(also tried 10uF) between NRST pin and ground. Microcontroller has an internal pullup. and it is showing 3.3V at the t...

image.png
Ragini by Associate II
  • 2594 Views
  • 5 replies
  • 0 kudos

STM32H7 Custom Project Schematic review help

Hi guys,I been working on this project for some time now on my "free time"...but so far without any success.In the first prototype I have assembled all the peripherals(QSPI, eMMC, SDRAM, some I2C and SPI slaves peripherals and DSI display.).Nothing s...

pema_0-1724698352193.png pema_1-1724698368494.png pema_2-1724698389561.png pema_3-1724698407578.png
pema by Associate II
  • 3234 Views
  • 5 replies
  • 4 kudos

DMA channel1 Stream 0-7 which channel to choose

Hi i m working on H732 timer1 as PWM and its working fine, but when I try to implement DMA on timer1, there is no waveform. I enclosed the DMA code below, as I declare an array of 10 PWM duty cycle values..i suspect it's the Timer1 channel1 stream th...

StanJerm_0-1725327735894.png
StanJerm by Associate III
  • 3269 Views
  • 6 replies
  • 0 kudos

Resolved! HardFault when using UART and DMA

Hi, I have a program running on a STM32U083RCT that is raising a HardFault when running at full speed, but when stepping through the code using a debugger the code appears to run correctly. I have a transceiver device connected to to USART2. I have a...

Jorgie by Associate III
  • 2151 Views
  • 2 replies
  • 0 kudos

Lora Basics Modem on STM32L073RZT6

Hello, I'm working on testing the LoRa Basics Modem V4, available in SWL2001 on github, and for now I've managed to generate the executable and download the program on the board I have, but nothing has appeared yet on The Things Network. I believe th...

stm32 GPIO input from mcp23017 interrupt

Hello,I'm working on a project involving an STM32F103 and a mcp23017 port expander.I've connected the mcp23017 INTA to PA15, no pull-up or down involved.I'm able to drive the mcp23017 via I2C, no problem about that.The problem I have is detecting the...

Resolved! Control amount of samples for timer STM32H7 via PWM?

Hello, I need to make 10 samples via Tim13 and PWM in STM32H7. I implemented the next script, but finally, on the oscilloscope, I saw about 50 samples every 0.1 sec. Do you know, how easily control the number of samples for Timer in stm32?       #inc...

Ronil by Senior
  • 4277 Views
  • 8 replies
  • 1 kudos

Resolved! UART Transmission on STM32 Nucleo-h723zg

 I am using STM32 Nucleo-h723zg for a UART serial transmission using UART4 and UART7. I have used UART4 only in my code to test since using both was not working. Still, nothing is showing on my RealTerm serial monitor. I used STM32 Cube IDE. I don't ...

SAW by Associate II
  • 3556 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.