STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN on STM32G0 Filter setup

Hello, is there any simple example for (STM32G0B1CBT6) or similar where I can simply filter int genration for eg. only for 0x505 id in standart mode. I tested many samples and I believe that there must be some bug in IDE. This is    static void MX_FD...

JD3 by Associate II
  • 4869 Views
  • 8 replies
  • 1 kudos

SPI MISO "broken" after a while

Hello,I have a Nucleo-F439ZI as SPI master connected to four Nucleo-F030R8 SPI slaves.Initially, the SPI communication was working perfectly fine. But after a while, the master received only zeros on MISO line even though, the slaves where sending da...

_Daniel_ by Associate II
  • 8868 Views
  • 18 replies
  • 8 kudos

STM32F405RGT6 USB DFU

Hi, I recently designed a custom stm32F405RGT6 board. However, I was unable to use the DFU mode.From what I understand, bootloader comes with DFU enabled. However, when I used stm32cubeprogrammer, it kept mentioning "DFU not detected". This is my sch...

MCU.png USB connection.png
Yeo by Associate
  • 3073 Views
  • 2 replies
  • 1 kudos

Resolved! Replacement for STM32H753ZI

Hi, I am looking for the STM32H series part with more GPIOs and Timers than STM32H753ZI. Can you please suggest me some of the options in H series?Below is my requirement GPIOSPII2CUARTTimerCANInternal ADC Channel6052216217

DJ7 by Associate
  • 1997 Views
  • 3 replies
  • 2 kudos

Resolved! QSPI connection in STM32L412

DEar forum I'm designing a system to use a quad spi memory for log purposes. And I see that the L412R8I only features qspi bank 1 on AF10Bank 0 is missingIs it okay? I'd only use it by indirect access, because the memory is to be read and written Are...

nachus001 by Associate II
  • 1997 Views
  • 3 replies
  • 0 kudos

Bug in CPAL_I2C_IsDeviceReady

Posted on January 30, 2014 at 08:24 There is a bug in CPAL_I2C_IsDeviceReady that prevents it from ever returning failure. /* wait until timeout elapsed or target device acknowledge its address*/ while ((__CPAL_I2C_HAL_GET_ADDR(pDevIn...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.