STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC + Sleep-now mode = problem

Posted on January 15, 2012 at 17:08 Hello. In my application i'm using RTC second interrupt (clock/calendar features) and RTC alarm event. I want the system to go into sleep-now low power mode (with all interrupts enabled and running) and wa...

Running user code from STM32F4's internal RAM

Posted on January 13, 2012 at 13:57Hi,I am new to ARM development, I just bought a STM32F4Discovery board and am experimenting with it. I was wondering if there was a way to load and run user code from the internal RAM; it would be very helpful if t...

multiple load in interrupts: any restrictions?

Posted on January 13, 2012 at 11:42Concerning the NVIC interrupt handler: I am a bit curious, how NVIC manages to keep log of the multi-load commands, if several interrupts would interrupt one each other. As far as I understand it, STM32 has 16 leve...

flyer31 by Senior
  • 3133 Views
  • 9 replies
  • 0 kudos

PE2 or PE3?

Posted on January 14, 2012 at 02:31Hi, On UM1472 - STM32F4DISCOVERY User Manual, page 27, says pin PE2 is connected to CS_I2C/SPI of LIS302DL. On schematics (page 30 and 35) the pin connected is PE3. Anyone knows what is the correct pin? Best regar...

jsmaia2 by Associate
  • 1054 Views
  • 1 replies
  • 0 kudos

PRIGROUP Initialization

Posted on January 13, 2012 at 14:56I can't figure out how the PRIGROUP is initialized in the stm32.  In PM0056 (Programming manual)  it appears the SCB_AIRCR register field for PRIGROUP is initial 0, but the table defining PRIGROUP (table 45) has no...

CrossWorks on Mac OS - ''cannot open USB device''

Posted on January 13, 2012 at 05:44My board connected to the computers USB ports powers up and runs the default LED demo.I have a simple CrossWorks project. When I double click on the ST-LINK/V2 Target, I get: ''cannot open USB device''Is there some...

ozvena by Associate II
  • 1155 Views
  • 2 replies
  • 0 kudos

16 bit result from ADC

Posted on January 07, 2012 at 17:13The original post was too long to process during our migration. Please click on the attachment to read the original post.

seba881 by Associate
  • 1884 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.