2012-01-12 8:44 PM
My board connected to the computers USB ports powers up and runs the default LED demo.
I have a simpleCrossWorks project. When I double click on the ST-LINK/V2 Target, I get: ''cannot open USB device''
Is there some prerequisite like STLINK driver I am missing?I can't find the answer anywhere, I spent hours looking…Thank you!2012-01-13 4:49 AM
Check Properties for the ST-LINK/V2 and make sure you are using SWD for the Target Interface Type, not JTAG.
Hope this helps.MAJ2012-01-13 6:47 AM
Thank you, that did the trick!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.