2012-01-12 4:30 AM
There is a part of codes in the stm324xg_eval_audio_codec.c.
/* CODEC_I2C SCL and SDA pins configuration -------------------------------------*/ /* If the I2C peripheral is already enabled, don't reconfigure it */ if ((CODEC_I2C->CR1 & I2C_CR1_PE) != 0) { GPIO_InitStructure.GPIO_Pin = CODEC_I2C_SCL_PIN | CODEC_I2C_SDA_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType =GPIO_OType_OD
; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(CODEC_I2C_GPIO, &GPIO_InitStructure); /* Connect pins to Periph */ GPIO_PinAFConfig(CODEC_I2C_GPIO,CODEC_I2S_SCL_PINSRC
, CODEC_I2C_GPIO_AF); GPIO_PinAFConfig(CODEC_I2C_GPIO,CODEC_I2S_SDA_PINSRC
, CODEC_I2C_GPIO_AF); } /* CODEC_I2S pins configuration: WS, SCK and SD pins -----------------------------*/ GPIO_InitStructure.GPIO_Pin = CODEC_I2S_WS_PIN | CODEC_I2S_SCK_PIN | CODEC_I2S_SD_PIN; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType =GPIO_OType_PP
; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(CODEC_I2S_GPIO, &GPIO_InitStructure); /* Connect pins to I2S peripheral */ GPIO_PinAFConfig(CODEC_I2S_GPIO, CODEC_I2S_WS_PINSRC, CODEC_I2S_GPIO_AF); GPIO_PinAFConfig(CODEC_I2S_GPIO, CODEC_I2S_SCK_PINSRC, CODEC_I2S_GPIO_AF); GPIO_PinAFConfig(CODEC_I2S_GPIO, CODEC_I2S_SD_PINSRC, CODEC_I2S_GPIO_AF); I want to know why I2C and I2S use different modes. By the way, I thinkCODEC_I2S_SCL_PINSRC
shoud be corrected toCODEC_
I2C
_SCL_PINSRC. #basic-electronics2012-01-12 4:45 AM
I2C has always been a bidirectional interface using open collector/drain, slave devices recognize when they are addressed and need to signal back to the master. Push-pull would cause drivers to fight/contend with each other.
I2S is a single slave, point-to-point interface, as I recall.2012-01-14 9:08 AM
''When I should set the GPIO to open drain mode or push-pull mode?''
You set whatever the application requires!''Open-Drain'', ''Open-Collector'' and ''Push-Pull'' are basic electronic terms - nothing specifically to do with the STM32. If you're not familiar with the terms, a basic electronics text book should help...
http://en.wikipedia.org/wiki/Push%E2%80%93pull_output
http://en.wikipedia.org/wiki/Open_collector
http://en.wikipedia.org/wiki/Open_drain
http://www.opamp-electronics.com/tutorials/digital_theory_ch_003.htm
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.