2012-01-10 4:31 PM
It's strange, I don't have a transmission with this function and I don't know why. State of registers after USART_Cmd
(
USART1,
ENABLE)
is: SR -> 0x000000C0 (OK) DR -> 0 BRR -> 0x00000683 (for HSI = 16 [MHz] -> OK) CR1 -> 0x0000200C (OK) CR2 -> 0 CR3 -> 0x00000300 (OK) GTPR -> 0 In step-by-step working (debug in keil) i see that for example 'A' isn't written to DR(DR is still 0) I tried change USART1 for USART2 but problem wasn't solved.void
USART1forFUN(
void
)
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
/* Enable GPIOA and USART1 clock */
RCC_AHBPeriphClockCmd(
RCC_AHBPeriph_GPIOA,
ENABLE)
;
RCC_APB2PeriphClockCmd(
RCC_APB2Periph_USART1,
ENABLE)
;
/* Connect P9 to USART1_Tx
* Connect P10 to USART1_Rx * Connect P11 to USART1_CTS * Connect P12 to USART1_RTS */ GPIO_PinAFConfig(
GPIOA,
GPIO_PinSource9,
GPIO_AF_USART1)
;
GPIO_PinAFConfig(
GPIOA,
GPIO_PinSource10,
GPIO_AF_USART1)
;
GPIO_PinAFConfig(
GPIOA,
GPIO_PinSource11,
GPIO_AF_USART1)
;
GPIO_PinAFConfig(
GPIOA,
GPIO_PinSource12,
GPIO_AF_USART1)
;
/* Configure USART Tx and Rx as alternate function push-pull */
GPIO_InitStructure.GPIO_Mode
=
GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed
=
GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType
=
GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd
=
GPIO_PuPd_UP;
GPIO_InitStructure.GPIO_Pin
=
GPIO_Pin_9|
GPIO_Pin_10|
GPIO_Pin_11|
GPIO_Pin_12;
GPIO_Init(
GPIOA,
&
GPIO_InitStructure)
;
/* USARTx configured as follow:
- BaudRate = 9600 baud - Word Length = 8 Bits - One Stop Bit - No parity - Hardware flow control enabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate
=
9600
;
USART_InitStructure.USART_WordLength
=
USART_WordLength_8b;
USART_InitStructure.USART_StopBits
=
USART_StopBits_1;
USART_InitStructure.USART_Parity
=
USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl
=
USART_HardwareFlowControl_RTS_CTS;
USART_InitStructure.USART_Mode
=
USART_Mode_Rx|
USART_Mode_Tx;
USART_Init(
USART1,
&
USART_InitStructure)
;
/* Odblokowanie USART1 */
USART_Cmd(
USART1,
ENABLE)
;
USART_SendData(
USART1,
'A'
)
;
while
(
USART_GetFlagStatus(
USART1,
USART_FLAG_TXE)
==
RESET)
;
USART_SendData(
USART1,
'B'
)
;
while
(
USART_GetFlagStatus(
USART1,
USART_FLAG_TXE)
==
RESET)
;
USART_SendData(
USART1,
'C'
)
;
while
(
USART_GetFlagStatus(
USART1,
USART_FLAG_TXE)
==
RESET)
;
USART_SendData(
USART1,
'D'
)
;
while
(
USART_GetFlagStatus(
USART1,
USART_FLAG_TXE)
==
RESET)
;
}
2012-01-12 4:56 AM
The read/write of DR go to different internal registers, ie you can't see what you wrote in. You could loop-back externally and wait for it to clock over.
Try disabling flow control (CTS/RTS), and see if the data is emitted. Use a scope on the pin to observed data.2012-01-12 7:15 AM
Thanks for help ~clive1, it was very good idea with loop-back :).
Now USART is working but I have another problem :\ when I clean [1] flag USART_FLAG_RXNE only before SECOND LED ON-OFF (after received 'O' from terminal), the 'K' can't be identified. Letter 'K' is recognized when I clean that flag additionaly in [2] (after SECOND LED ON-OFF).USART_SendData(USART2, 'A');
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData(USART2, 'T'); while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData(USART2, 0x0D); while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); USART_SendData(USART2, 0x0A); while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); /*FIRST LED ON-OFF */ GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET); Delay(50); GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_RESET); /* WAIT FOR 'O' */ while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) != RESET); while(USART_ReceiveData(USART2)!= 'O'); USART_ClearFlag(USART2, USART_FLAG_RXNE); //[1] /*SECOND LED ON-OFF */ GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_SET); Delay(50); GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_RESET); USART_ClearFlag(USART2, USART_FLAG_RXNE); //[2] /* WAIT FOR 'K' */ while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) != RESET); while(USART_ReceiveData(USART2)!= 'K'); USART_ClearFlag(USART2, USART_FLAG_RXNE); I would be very thankful for help.2012-01-12 5:00 PM
You need to wait for RXNE before reading each character, you do not need to clear RXNE, it is cleared by reading the data.
/*FIRST LED ON-OFF */
GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_SET);
Delay(50);
GPIO_WriteBit(GPIOB, GPIO_Pin_6, Bit_RESET);
/* WAIT FOR 'O' */
do
{
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET);
} while(USART_ReceiveData(USART2)!= 'O');
/*SECOND LED ON-OFF */
GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_SET);
Delay(50);
GPIO_WriteBit(GPIOB, GPIO_Pin_7, Bit_RESET);
/* WAIT FOR 'K' */
do
{
while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET);
} while(USART_ReceiveData(USART2)!= 'K');
2012-01-13 4:01 AM
It's strange when delete line [1] and [2] program doesn't work good in normal mode . STM32L can receive 'O' but no 'K'. There is one exception: when I'm working in keil debug mode and stop program after receiving 'O' and then resume, STM32L receive 'K' :\
I think that the problem is with Delay() function. When I comment this line project works good. But I don't have idea how Delay() have impact on USART. Delay() is standard implementation from STM32L Discovery Demo: void Config_Systick(void) { RCC_ClocksTypeDef RCC_Clocks; RCC_GetClocksFreq(&RCC_Clocks); SysTick_Config(RCC_Clocks.HCLK_Frequency / 100); } void Delay(uint32_t nTime) { TimingDelay = nTime;while(TimingDelay != 0);
} void TimingDelay_Decrement(void) {if (TimingDelay != 0x00)
{ TimingDelay--; } } void SysTick_Handler(void) { disableInterrupts(); TimingDelay_Decrement(); enableInterrupts(); }2012-01-13 5:10 AM
I hope you figure it out, I'm not good with incomplete code fragments.
Look carefully at the code I provided, consider not using interrupts/delays, consider toggling the LEDs as characters arrive, not pulsing them.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.