STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! External oscillator input

In application we are using MCU part no STM32G0KCIU6 of LQFP32 / UFQFPN32 - GP package, can external oscillator of frequency 16MHz (Example: Part no ASEMB-16.000MHZ-LY-T) can be connected to pin no 2 which is dedicated for LSE clock frequency 32KHz. ...

STM32F103 CAN CYCLE TIME

Hi,I am STM32F103 with 72Mhz clock and am trying to send the CAN messages (MCP2561 as CAN transceiver) with 500kbps and am using CAN BUS ANALYZER to check the CAN msgs.Here am sending 3 CAN msgs for every 100ms using timer interrupt but some times s...

HRedd.1 by Associate II
  • 1651 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H753 - Unused USB connection

Hi Team, we are using the STM32H753VI in our design.we are not using the USB interfaces.In this case, what is the termination to be done to the VDD33USB pin of STM whether it can be NC, GND? ThanksManikandan R

Resolved! FDCAN Configurations to Transmit Data in Classic mode

Devkit - NUCLEO-H563ZI IDE - STM32CubeIDE Version: 1.16.1 Build: 22882_20240916_0822 (UTC) Details - Trying to create a sample program for FDCAN in which the program transmits the data using the CAN protocol. I have tried different methods but was no...

mayank__ by Associate II
  • 5403 Views
  • 8 replies
  • 0 kudos

Resolved! Output voltage

Wanted to confirm if the input/output voltage is 3.3V or 5V depending on the I/O structure of my pin . I scoped a PWM signal with the board connected to the PC and on the dedicated pin I see the signal in  mV. I would like to send a higher voltage th...

Marrkinho by Associate II
  • 5487 Views
  • 2 replies
  • 3 kudos

Resolved! ST-Link driver issue

Hi All,I would need the link to download the ST-Link driver 2.1.0.0 from 08/06/2017.The latest one is interrupting the connection to board randomly every couple of seconds.I cannot find any link to the former ST-Link drivers, so please provide me the...

Sebdee by Associate II
  • 2381 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.