2024-08-26 6:02 AM
Hi All,
I would need the link to download the ST-Link driver 2.1.0.0 from 08/06/2017.
The latest one is interrupting the connection to board randomly every couple of seconds.
I cannot find any link to the former ST-Link drivers, so please provide me the aforementioned one.
Thanks.
Solved! Go to Solution.
2024-10-18 1:53 AM
Hi All,
I have solved the problem. The issue was coming from an old USB extension cable I had to connect the USB HUB to it. I have replaced this 50cm extension cable with a newer one and now it works with the latest driver.
What is still strange, is that when I connect the board directly to another single USB port on my computer, either USB 3.X or 2.X, with a new cable, this does not work. I must pass through a HUB to make it work.
Thanks
2024-08-26 6:46 AM
Welcome @Sebdee, to the community!
version 2.1.0.0 is very old and no longer up-to-date. There are some websites that deal with Bluepill and similar things and juggle with such old drivers, but this cannot be a clean solution.
Which board with which STM32 shows the behaviour with the interruptions in connection with which software?
Regards
/Peter
2024-08-26 7:19 AM
Hi @Peter BENSCH ,
Thanks. I am using an STM32 Nucleo-F767 ZI. Up to last week everything was fine.
However, now when I connect the board to the USB port, the LD4 stays green (instead of red), and the board resets randomly and the LD4 is blinking, like when you program the board. I guess this is linked to the ST-Link. Also, when I am in STM32CubeProgrammer, the board can connect, but randomly it lost the connection with the message "Connection to device 0x451 is lost".
When I plug the same board to another computer, the LD4 is red and not green and it works perfectly without any issue. The only difference I could find between both computers was the ST-Link driver versions between them. The machine with version 2.1.0.0 works smoothly.
Thanks
2024-09-20 5:08 AM
Hi All,
I have tried with the driver version 2.1, but it still fails...
Does anyone would know why it does not work on one of my computer?
I am sur it has to do with the USB ports, that perhaps cannot maintain enough power.
I have tried with all types of USB ports (2.x, 3.x), but the behavior is always the same.
2024-10-18 1:53 AM
Hi All,
I have solved the problem. The issue was coming from an old USB extension cable I had to connect the USB HUB to it. I have replaced this 50cm extension cable with a newer one and now it works with the latest driver.
What is still strange, is that when I connect the board directly to another single USB port on my computer, either USB 3.X or 2.X, with a new cable, this does not work. I must pass through a HUB to make it work.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.