STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two Resets Required for STM32G474

Hello All, I'm having a problem with an STM32G474 on a custom board. Overview of FaultFirst, weird behavior of the IWDG was observed. A hard fault was generated intentionally after 10 seconds of run time and no reset behavior was observed. Then, a wh...

RyanColeman_0-1729211736247.png RyanColeman_1-1729211747965.png

Read Systick Timer Value Directly for 1ms Timebase

Hi, I am working on a project on the STM32H730 that runs a high priority audio interrupt thread as well as a lower priority asynchronous loop for user interface processing and a 1ms SysTick interrupt for user interface processes that need some accura...

EPala.2 by Senior
  • 8440 Views
  • 17 replies
  • 0 kudos

Resolved! How to enable/disable Flash Write Protection?

Hi guys,I am read the example "STM32Cube_FW_F1_V1.8.4\Projects\STM32F103RB-Nucleo\Examples\FLASH\FLASH_WriteProtection", and want to rewrite it on my board.my code is as follows:  HAL_FLASH_Unlock(); HAL_FLASH_OB_Unlock(); HAL_FLASHEx_OBGetCo...

Junde by Senior III
  • 7062 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with I2C4 on STM32H745I-Disk

I have two codes, one only with the I2C4 communication working and the other code besides the I2C has the display but in this one the I2C communication does not work, what could be happening?With a logic analyzer I can see that in both codes the cloc...

Resolved! STM32F410: ITRx "reserved"?

Hi guys,can someone please explain the internal trigger connections for the stm32f410 controllers to me?According to the referance manual (RM0401, see below) only TIM1 and TIM5 can be configured as slave timers with just ONE possible internal trigger...

ITR.png

Powering STM through USB-C port

Hi,I want to power a STM32Ux based board using USB-C port. I am required to use two numbers of  a Type-A to USB-C type of cable and also it should support USB-C to USB-C type of cable in OR ring. Max load current of the board is less 1.5A. I am looki...

SKCL-1 by Associate II
  • 1958 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.