STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MISO line tri-state issue for STM32H573AII3Q

Hello, We are using STM32H573AII3Q in our application. One external IC is interfaced with this uC through SPI lines.  We are observing a tristate on MISO line. To investigate we isolated the uC and checked the MISO line. It is having a voltage level ...

madhu1_0-1728542550473.png
madhu1 by Associate II
  • 3225 Views
  • 5 replies
  • 0 kudos

OpenAMP automatic address assignment

Hello I'm developing RTOS environment of dual-core in STM32H757.In OpenAMP communication mode, CM4 is the master and CM7 is the slave, and I used SRAM4 to create SHMEM.I could refer to the examples provided by STM32, and I read the application note A...

StrangeTau_0-1729476801672.png StrangeTau_1-1729476845842.png StrangeTau_2-1729476901562.png

Function OPENAMP_send Error

Hello Error Definition1 : the return value of the OPENAMP_send function is 4. // RPMSG_ERR_NO_MEM?Error Definition2 : the return value of the OPENAMP_send function is -2007. // RPMSG_ERR_ADDR I'm developing RTOS environment of dual-core in STM32H757....

StrangeTau_0-1729210018747.png StrangeTau_4-1729210221865.png StrangeTau_2-1729210019216.png StrangeTau_3-1729210018765.png

jump to FreeRTOS appl is failed

Hi,I'm developing a custom bootloader.My freertos appl. is running well on debug mode in stm32cubeide while my freertos appl is on 0x08008000.MEMORY{RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K - 8/*FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 512K*/F...

Paul.Lee by Associate III
  • 1943 Views
  • 2 replies
  • 0 kudos

STM32H723 RS-485

Hi,I am trying to create a reliable communication in a noisy environment using RS-485 between 2 STM32 boards, one with STM32F302 that is receiving data from several sensors, performs some calculations and then send the data to a STM32H723 Board. On b...

Resolved! STM32G431 Comparator output to Timer

Hello.STM32G431CBT6Is it possible to route the output from the comparator to the input of the Timer input? The reference manual says that this is possible, but there is no description. And in the comparator register there are no options for choosing ...

Resolved! Writing data from RAM to Flash with DMA

Hello,  i'm wondering if it is possible to copy data from RAM to flash using DMA after unlocking the FLASH memory   static const uint32_t src[4] ={80,20,30}; static uint32_t dst = 0x080E0000; __HAL_RCC_DMA1_CLK_ENABLE(); dma_handler.Instance = DMA1...

Can't get Input Capture mode to work

I want to use input capture mode in my stm32l432kc nucleo-32 board to measure the length of a signal from a sensor of mine. I have set it up the following way:int main(void) { // ... MX_USART2_UART_Init(); MX_TIM16_Init(); HAL_TIM_IC_Start_IT...

DavidL_ by Associate III
  • 2149 Views
  • 4 replies
  • 0 kudos

STM32F1 I2C DMA has no stop bit

Hi. First time using this forum.I'm using an STM32F103C8 (genuine, not bluepill clone).I've easily used DMA to take sensor data and store it in a buffer, this has worked without issue (see below): void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { if ...

triqstar_2-1729419784722.png triqstar_3-1729419868264.png triqstar_4-1729419879486.png
triqstar by Associate
  • 942 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.