2013-04-22 4:28 PM
When executing the audio clip from flash[const defined location as in the example project] the audio file plays fine, but if I remove the ''const'' as to allocate ram for the audio clip, I get only a small block of white noise...I'd figure that given the DMA configured as memory-to-peripheral there to be no issue...looking at the output with a logic analyzer, the bytes appear to be the same in both conditions[audio clip executed from flash, and when from ram]...any suggestions as to what could be the subtle difference causing the problem would be much appreciated...
2013-04-22 4:30 PM
...this is when using the Stm32F4Discovery board and keil included example code...
2013-04-23 10:07 AM
most likely a timing issue
reading const data (from flash) incurs some latency (section 3.4.1)2013-05-02 8:35 AM
It was a timing issue with how I was sending the data -- I'd send single blocks of data for which the code was powering down the codec after each block, then re-initializing when processing again which needed to be corrected :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.