2013-05-02 10:20 AM
i am trying to interface gsm module , I want to use USART2 and USART3 ...
but I am not getting how to do that can anyone suggest me ... thank you .. iam attaching the code i am using in the attachments . #rs232-discovery-max3232-usart #tldr2013-05-02 10:35 AM
Figure out what pins you plan on using. Determine if the external peripherals need to connect at CMOS Serial levels, or RS232 levels.
Insufficient data here. STM32L USART3, try2013-05-02 10:40 AM
sorry , I think u ddnt see my attachment in this post ...
iam attaching my program file here .. ________________ Attachments : yogesh.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzZg&d=%2Fa%2F0X0000000bNj%2FVxmca7uQTMvJvT.IeSCxWIpIcrCTDS.1vo9FZSOcAPY&asPdf=false2013-05-02 10:42 AM
2013-05-02 10:48 AM
If you're using PB10/11, then you'll need to enable the GPIOB clock also.
Enable APB1 clocks for USART2 and USART32013-05-02 11:02 AM
sorry , I think u ddnt see my attachment in this post ...iam attaching my program file here ..
Sorry, I saw, a lot to wade through. Doesn't really describe the connectivity, and failure. The STM32L-Discovery has no serial ports attached, need to be more explicit about how this is wired up, and to what (part#, pin designations, not generic description). Should have this separate from code, ie summary. Try to evaluate USART function outside core application, then integrate.2013-05-02 11:10 AM
2013-05-02 11:12 AM
From other thread, blind mod for USART2
// sourcer32@gmail.com - STM32L15x USART2 Demo 9600 8N1
#include ''stm32l1xx.h''
void main(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Assumes CMSIS and SystemInit() set up clocks before calling main() */
/* Enable GPIO A clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Enable USART2 clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* Configure USART Rx & Tx as alternate function */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Mux out USART2 Rx & Tx */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); // PA2 USART2_TX
GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2); // PA3 USART2_RX
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_None;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
/* USART configuration */
USART_Init(USART2, &USART_InitStructure);
/* Enable USART */
USART_Cmd(USART2, ENABLE);
while(1)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); /* Waitwhile TX full */
USART_SendData(USART2, 0xAA);
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.