2011-07-07 9:18 PM
I am trying to generate a single pulse using the TIM_SelectOnePulseMode() function in STM32f10x_tim.c source file. But I am not able to get the pulse. why?
I am using TIM4 CH2... Any advice? int main(void) { TIM_Cmd(TIM4, DISABLE); RCC_Configuration(); GPIO_Configuration(); PrescalerValue = (SystemCoreClock / 24000000) - 1; TIM_TimeBaseStructure.TIM_Period = 65535 TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 16383 TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC2Init(TIM4, &TIM_OCInitStructure); TIM_Cmd(TIM4, ENABLE); TIM_SelectOnePulseMode(TIM4, TIM_OPMode_Repetitive); return 0; } void RCC_Configuration(void) { RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOD, ENABLE); RCC_APB1PeriphResetCmd(RCC_APB1Periph_TIM4, ENABLE); } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOD, &GPIO_InitStructure); } #timer-one-shot #one-pulse #stm32 #tim42011-07-07 9:32 PM
which STM32 you are using?? the exact part no??
2011-07-07 10:26 PM
i'm using STM32F100B-eval...
2011-07-08 12:46 AM
for one pulse you have to do
/* One Pulse Mode selection */ TIM_SelectOnePulseMode(TIM2, TIM_OPMode_Single); but you are doing TIM_SelectOnePulseMode(TIM4, TIM_OPMode_Repetitive); Please find here attached an example source code for generating one pulse. Hope it will help. Rgds, Rosarium ________________ Attachments : OnePulse.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1D8&d=%2Fa%2F0X0000000bjt%2FDDx0jf4tKrrBNem0inHVER9iZcqPyjb2YZcYTDmAE5w&asPdf=false2011-07-08 12:56 AM
2011-07-08 1:13 AM
thanks! but erm, it didn't matter if i used ''single'' or ''repetitive'', there was still no output at my TIM4. And is the input capture mode necessary? since I just need to output pulses...
2011-07-08 1:33 AM
Yes input capture is also necessary.
Following is an example for TIM2 as attached last time.int main(void)
{ /* System Clocks Configuration */ RCC_Configuration();/* Configure the GPIO ports */
GPIO_Configuration();/* TIM2 configuration: One Pulse mode ------------------------
The external signal is connected to TIM2_CH2 pin (PA.01), The Rising edge is used as active edge, The One Pulse signal is output on TIM2_CH1 pin (PA.00) The TIM_Pulse defines the delay value The (TIM_Period - TIM_Pulse) defines the One Pulse value. The TIM2CLK is fixed to 72 MHz, the Prescaler is 1, so the TIM2 counter clock is 36 MHz. The Autoreload value is 65535 (TIM2->ARR), so the maximum frequency value to trigger the TIM2 input is 500 Hz. The TIM_Pulse defines the delay value, the delay value is fixed to 455.08 us: delay = CCR1/TIM2 counter clock = 455.08 us. The (TIM_Period - TIM_Pulse) defines the One Pulse value, the pulse value is fixed to 1.365ms: One Pulse value = (TIM_Period - TIM_Pulse)/TIM2 counter clock = 1.365 ms. ------------------------------------------------------------ *//* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
/* TIM2 PWM2 Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 16383; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;TIM_OC1Init(TIM2, &TIM_OCInitStructure);
/* TIM2 configuration in Input Capture Mode */
TIM_ICStructInit(&TIM_ICInitStructure);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0;TIM_ICInit(TIM2, &TIM_ICInitStructure);
/* One Pulse Mode selection */
TIM_SelectOnePulseMode(TIM2, TIM_OPMode_Single);/* Input Trigger selection */
TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);/* Slave Mode selection: Trigger Mode */
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Trigger);while (1)
{} }2011-07-08 4:54 AM
I am trying to generate a single pulse using the TIM_SelectOnePulseMode() function in STM32f10x_tim.c source file. But I am not able to get the pulse. why?
I am using TIM4 CH2... Any advice?
Well for starters, to get TIM4_CH2 out of PD13, you are going to need to enable the AFIO peripheral and Remap the TIM4 to use those pins. If your board/part isn't using PD13, then you'll need to enable the appropriate pin (PB7 ?)
2011-07-10 7:22 PM
ok, now I have changed to TIM2 CH1 (PA0) which coincides with the wakeup.
I have enabled my AFIO and re-mapped my TIM2 CH1, but I am still not getting it. Why? here's my code. // ****************************************************************************** #include ''stm32f10x.h'' TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; TIM_OCInitTypeDef TIM_OCInitStructure; void RCC_Configuration(void); void GPIO_Configuration(void); int main(void) { RCC_Configuration(); GPIO_Configuration(); TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 16383; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM2, &TIM_OCInitStructure); TIM_ICStructInit(&TIM_ICInitStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0; TIM_ICInit(TIM2, &TIM_ICInitStructure); TIM_SelectOnePulseMode(TIM2, TIM_OPMode_Single); TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2); TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Trigger); while (1) {} } void RCC_Configuration(void) { SystemInit(); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinRemapConfig(GPIO_FullRemap_TIM2, ENABLE); } #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file, uint32_t line) { while (1) {} } #endif2011-07-10 7:33 PM
hi, i tried copy-and-paste your code to see if works, but i'm still not getting a pulse.
and i received another reply from another user that I should enable AFIO and remap, so please see my code below: #include ''stm32f10x.h'' TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStructure; TIM_OCInitTypeDef TIM_OCInitStructure; void RCC_Configuration(void); void GPIO_Configuration(void); int main(void) { RCC_Configuration(); GPIO_Configuration(); TIM_TimeBaseStructure.TIM_Period = 65535; TIM_TimeBaseStructure.TIM_Prescaler = 1; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM2; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 16383; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM2, &TIM_OCInitStructure); TIM_ICStructInit(&TIM_ICInitStructure); TIM_ICInitStructure.TIM_Channel = TIM_Channel_2; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0; TIM_ICInit(TIM2, &TIM_ICInitStructure); TIM_SelectOnePulseMode(TIM2, TIM_OPMode_Single); TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2); TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Trigger); while (1) {} } void RCC_Configuration(void) { SystemInit(); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE); } void GPIO_Configuration(void) { GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinRemapConfig(GPIO_FullRemap_TIM2, ENABLE); } #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file, uint32_t line) { while (1) {} } #endif --------------------------------------------------------------------------------- what am i doing wrong here? i can't seem to get the code no matter how i try. please help... much appreciated.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.