STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2s USART conflict??

Posted on May 13, 2013 at 00:12I am successfully using I2C control and I2S to send data to the CS43L22 and producing simple sawtooth--> musical notes(see http://www.mind-dump.net/configuring-the-stm32f4-discovery-for-audio#comment-1344). When I try ...

pccmd by Associate II
  • 1652 Views
  • 3 replies
  • 0 kudos

STM32F4Discovery FAT FS

Posted on May 04, 2013 at 06:01I am trying to implement at FAT FS on the STM32F4 Discovery board...the firmware package provided by st supplies third party files.  But are these files enough to implement the FAT FS on the STM32F4 board? Or is there ...

ADC via dma and USART

Posted on February 13, 2013 at 10:52 Hello, i am having trouble writing code on STM32F4Discovery. my goal is to get values from ADC in continuous mode and send them to USART/UART (with DMA or without)using interrupts. so i wrote a code made out ...

Continuous data reading from USART

Posted on May 13, 2013 at 00:53Hello,I have a USART data that comes from another device that runs continuously, I have to read all of this data and send it directly to a PC host through a USB.The problem is that I don't want to loose any received da...

slachist by Associate II
  • 1268 Views
  • 1 replies
  • 0 kudos

STM32F4 running hot

Posted on May 11, 2013 at 10:43hello my sth32f4 discovery is mcu is running hot and u1 is hot also what is going on??

Calculate Temperature Sensor STM32L Discovery

Posted on May 11, 2013 at 19:44hi , I have a question , when I  calculate the temperature with this code using the formulate in the data sheet:val_adc=ADC_GetConversionValue(ADC1); vsense=(val_adc*Vref)/0xfff;val_adc=(vsense/Avg_Slope)-273.15;in the...

kotoel26 by Associate II
  • 1306 Views
  • 2 replies
  • 0 kudos

STM32 Cannot read GPIO status

Posted on May 11, 2013 at 10:46 I've been trying for a week now, but I can't seem to read the status of the GPIO ports of the STM32F103RB. can turn LED's on, and transmit CAN, but really struggling to see what the issue is with this one. newish ...

rob by Associate
  • 1760 Views
  • 2 replies
  • 0 kudos

STM32F4 SPI Clock polarity - How to change it dynamically?

Posted on May 09, 2013 at 22:50We can initialize the SPI port clock polarity  by :- SPI_InitStruct.SPI_CPOL = SPI_CPOL_Low; SPI_InitStruct.SPI_CPHA = SPI_CPHA_1Edge; If we have several slaves connected to the SPI port, different slave operated using...

shinseow by Associate
  • 3115 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.