STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32w108cu64 can't initialize the internal regulators?

Posted on January 18, 2014 at 08:29Hi all, recently I layout a pcb with stm32w108cu64(copy from the MB954 Zigbee Domoboard)But it seems doesn't work. I try to use ST flash loader to connect the board, but fail. The I measure the VREG_OUT is 1.786V a...

0690X000006054WQAQ.png 0690X00000604zNQAQ.png
lmgames by Associate II
  • 2174 Views
  • 4 replies
  • 0 kudos

Determine how 'busy' cpu is?

Posted on January 20, 2014 at 16:44I'm on an STM32 F2, but a generic idea would be ideal :) Is there any way to get a high level 'reasonably' accurate idea of how busy the cpu? Given the variety of peripherals and so on I'm sure its quite a challeng...

skeezix by Associate II
  • 1874 Views
  • 4 replies
  • 0 kudos

STM32 F4 Discovery Demo

Posted on January 17, 2014 at 21:44I've got a STM32 F4 discovery board for STM32F401with the 9 axis sensors on it. I want to open up the demo project using Keil uVision 4 and modify it. I'm getting an error as soon as I open the project that says Er...

munger by Associate II
  • 2976 Views
  • 4 replies
  • 0 kudos

FAT FS

Posted on November 01, 2013 at 09:51Hi, Can anyone give me some help/advice on how to go about implementing Chan's FAT FS? I'm using MikroC Pro for ARM as my toolchain so things are going to be little bit different from most of the toolchains used o...

flash CRC integrity

Posted on January 15, 2014 at 21:14Hello, I know this has been discussed before, but reading through it all, I am still unable to grasp the solution of my problem: What I am trying to do is check the integrity of the flash (code) on the STM32L1xx ch...

klemen by Associate II
  • 13661 Views
  • 14 replies
  • 0 kudos

Issue with PWM TIM3 on STM32F3Discovery board

Posted on January 17, 2014 at 18:31 Hi all, I'd like to see a PWM with my oscilloscope, but I see nothing and I can't understand why. Can you help me? Thanks in advantage <I> int main(void) { TIM_Config(); GPIO_Configurati...

Program doesn't run with Debug detached

Posted on January 16, 2014 at 16:40I have a STM32F415VG which I have on my own board. The program code all runs when I have my SW debug adapter hooked up, but if I try to run the program without the adapter connected, nothing works. My oscillator do...

TIM flags automatically set when TIM enabled

Posted on June 19, 2013 at 16:16Hello, I am facing a problem with the timers I am using in STM32f100 MCU. I have configured different timers to operate during the execution of the code, but somehow, all the flags related to Capture/compare or Update...

0690X00000602kvQAA.jpg
rachit by Associate
  • 1170 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.