STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

warning marker for vcp program

Posted on January 17, 2014 at 23:28Hey Guys, After I programed vcp for STM32F427 Eval board by following the example of STM32F429Discover board, but when I plug it into the PC, The PC can find it but always get a warning marker on the Device manager...

0690X00000602qrQAA.jpg
kqian by Associate II
  • 2112 Views
  • 10 replies
  • 0 kudos

Assembly Code Example

Posted on May 01, 2013 at 00:02I've made up a board and embedded a STM32F4 on it.  I want example assembly code to compile and upload to the chip.  I can't find any on the entire internet for a Cortex-M4.  Does anyone have a link to a generic GPIO b...

drobison by Associate II
  • 10298 Views
  • 25 replies
  • 0 kudos

STM32F401CC Clock configuration

Posted on January 21, 2014 at 18:00Hello,We are developping an application on STM32F401CC mcu and we are not sure that our clock configuration is correct because, when we are setting baud rate of USART1 or USART2 greater than 115200 bps, data exchan...

vincent by Associate II
  • 1599 Views
  • 1 replies
  • 0 kudos

STM32F0 SWD Lockout

Posted on January 20, 2014 at 19:43 Hi Everybody, i'm trying to get some of the STM32F0 peripherals (in this case GPIO, SysTick, NVIC, SPI, DMA) working. Im using IAR EW 6.7 + IAR I-Jet (which is connected via SWD to the Chip). A...

twalter by Associate II
  • 1620 Views
  • 3 replies
  • 0 kudos

USB virtual COM port hot plug problem

Posted on October 17, 2012 at 16:58Hi,I have a problem while developing a USB-to-serial device and I am looking for a solution.I successfully implemented a USB virtual COM port on STM32F407 microcontroller. I can send and receive data to/from the co...

yesralph by Associate
  • 3538 Views
  • 6 replies
  • 0 kudos

STM32f10x WWDG ''Window WatchDog Timer''

Posted on January 21, 2014 at 13:46Hello    I am using STM32f103RET6 in my project. This project is very important and device should never stop working. Also device is remote and it is not possible to reset it easily. I try to use WWDG for unforesee...

stm32f3discovery

Posted on January 20, 2014 at 11:43Hi,I have a problem with the STM32F3Discovery because i want to capture the signal of the board to watch and display it on my PC. I am using ''Keil'' programm, but i'm not able to do it. Is there someone who could ...

v2 by Associate
  • 1741 Views
  • 3 replies
  • 0 kudos

stm32l151 not transmitting

Posted on January 21, 2014 at 04:13Hi, this is my first post and first time working on an stm, so I am a bit new to this. I have a circuit I have been working on as a hobby. When the circuit is receiving, it is getting data from a device, and when i...

ADC , DMA , TIM8 Triggering

Posted on January 03, 2014 at 06:45 Hi, I am attempting to use timer 8 to trigger adc sampling using stm32f1. I have referred to some example on the forum from Clive1 which is using timer 1 . However the code does not work when i c...

STM32F415 bus fault's with random adress

Posted on January 21, 2014 at 07:45Hello, I use stm32f415 and have bus fault with random adress. For example the content of BFAR register is 0x268dfb8; 0Ñ…4B404288; today i have 0xE000ED38. And frequency of bus fault change when I change the priorit...

flauwear by Associate
  • 1297 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.