2014-01-17 9:31 AM
Hi all,
I'd like to see a PWM with my oscilloscope, but I see nothing and I can't understand why. Can you help me? Thanks in advantage <I>int main(void)
{
TIM_Config();
GPIO_Configuration();
/* Infinite loop */
while (1)
{
}
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOB clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_2); // TIM3 Channel1 PA6 AF2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // Or UP for open-collector sources
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
/********************************/
static void TIM_Config(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
__IO uint16_t CCR1_Val = 40961;
uint16_t PrescalerValue = 0;
/* TIM3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
/* ----------------------------------------------------------------------- */
TIM_DeInit(TIM3);
/* Compute the prescaler value we want TIM3 clk @8Mhz => Presc = 8*/
PrescalerValue = (uint16_t) ((SystemCoreClock) / 8000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 100;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Output Compare Timing Mode configuration: Channel1 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = CCR1_Val;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC1Init(TIM3, &TIM_OCInitStructure);
TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* TIM3 enable counter */
TIM_Cmd(TIM3, ENABLE);
}
</I>
2014-01-17 9:32 AM
BTW do you know how hlm format the code as code?
2014-01-17 9:43 AM
Hi
I think you want : /* Output Compare Timing Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; or the PWM22014-01-17 10:09 AM
You use the Paintbrush [<>] icon (top left)
Your problem here is that with a period of 100 you're never going to get the counter to reach 40961 Set TIM_TimeBaseStructure.TIM_Period = 100-1; // Divide by 100 .. TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_Pulse = 50; // 100/2 is 50/50 duty2014-01-18 5:22 AM
Thank you but it doesn't work both with new period/pulse (100-1/50) and
<> TIM_OCMode = TIM_OCMode_PWM1 </>Any other idea?2014-01-18 6:23 AM
Is PA6 clashing with the L3GD20 (SAO/SDO)?
Can't you use PA4 (TIM3_CH2)?2014-01-18 6:31 AM
I'm just trying with TIM3_CH2 and let you know soon
2014-01-18 6:42 AM
Used TIM3_CH2 but it doesn't work, I reported the last code revision since I've lightly modified:
any ideas?#include ''main.h''
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
uint16_t PrescalerValue = 0;
static void TIM_Config(void);
void GPIO_Configuration(void);
int main(void)
{
/* TIM Configuration */
TIM_Config();
GPIO_Configuration();
/* Compute the prescaler value */
PrescalerValue = (uint16_t) ((SystemCoreClock) / 1000000) - 1;
/* Time base configuration */
TIM_TimeBaseStructure.TIM_Period = 100-1;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* Prescaler configuration */
TIM_PrescalerConfig(TIM3, PrescalerValue, TIM_PSCReloadMode_Immediate);
/* Output Compare Timing Mode configuration: Channel2 */
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_Pulse = 50;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OC2Init(TIM3, &TIM_OCInitStructure);
TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Disable);
/* TIM3 enable counter */
TIM_Cmd(TIM3, ENABLE);
/* Infinite loop */
while (1)
{
}
}
static void TIM_Config(void)
{
/* TIM3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
}
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOB clock enable */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_2); // TIM3 Channel2 PA4 AF2
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; // Or UP for open-collector sources
GPIO_Init(GPIOD, &GPIO_InitStructure);
}
2014-01-18 7:05 AM
2014-01-18 10:41 AM
Have you an example code for TIM stm32f3?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.