STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC initailization problem on STM32L series

Posted on March 20, 2014 at 13:52Hi, I am trying to use ADC for reading the voltage on pin A4.. I wrote an initialization method, however it get stuck in the last WHILE. Here there is the code: void ADC_Initialize(void) {   ADC_InitTypeDef  ADC_Ini...

luca2 by Associate II
  • 1102 Views
  • 1 replies
  • 0 kudos

SIP Stack for STM32F4

Posted on March 19, 2014 at 10:19I want to build a VoIP Phone ith STM32F4. Does anybody know, if there is a small SIP-Stack that can easily used with microcontroller. Thanks Marc #cross-post

doebber2 by Associate II
  • 1859 Views
  • 2 replies
  • 0 kudos

SPI TI mode

Posted on March 19, 2014 at 10:49Hello,could somebody explain me what is TI mode in SPI? Thank you #ti-mode #spi

karolina by Associate II
  • 2621 Views
  • 2 replies
  • 0 kudos

General question about DMA

Posted on March 18, 2014 at 22:45Hello everyone, i have a few general questions about DMA and i will appreciate the help if someone could answer to my questions. I know it is used to transfer data at high speeds between memory and peripherals, or me...

arganasss by Associate II
  • 1490 Views
  • 2 replies
  • 0 kudos

DAC problem with STM32F4

Posted on March 17, 2014 at 18:51Dear All,I have tested the DAC example on the STM32F429 and I have understood the way using / driving the DAC on the STM32F4. I have tried to create my sample code using the STM32F429 Discovery template, but nothing ...

I2C and sensors

Posted on March 19, 2014 at 16:08Hello, I have a STM32F100RBT6B board, and I should use some sensors LSM303D with I2C. Just a question: wich is the maximum number of sensors that I can use with an I2C interface? #sensor #i2c

I2C1 for STM32F100RBT6B

Posted on March 17, 2014 at 13:06Hi, I am using STM32F100RBT6B discovery board and I need to use I2C1 bus. I saw on datasheet that gpio PB6 and PB7 should be used for clock and data. I think to use PB8 and PB9 for the alimentation. Is it correct? N...

Stm32Cube FSMC address pin definiton bug

Posted on March 17, 2014 at 16:18Hello everybody! I check the Stm32Cube graphical pin definition. I want to use FSMC bus SRAM1, with 16 bit bus, and 1 address bit. The address pin I want is PE3, but the cube not allowing use this. If i use 1 bit add...

totti001 by Associate II
  • 1337 Views
  • 3 replies
  • 0 kudos

USART doesn't transmit first character

Posted on March 25, 2013 at 12:30Hi,I have a problem with transmitting character through USART3 port in STM32F207.Here there is the USART configuration code:--------------USART_DeInit(USART3);USART_InitStructure.USART_BaudRate = 115200;USART_InitStr...

lorbek by Associate II
  • 5901 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.