STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clear of EXTI-PR Flag at the the end of ISR doesn´t work

Posted on March 21, 2014 at 13:29Hello all, I am using a STM32F2xx chip. I found I strange behaviour in the interrupt service routine for the external interupts. Due to possible glitches in the edges triggering the external interrupt, I clear the pe...

andywild2 by Associate III
  • 1611 Views
  • 2 replies
  • 0 kudos

Error communication

Posted on March 19, 2014 at 15:16to be migrated, sourceId: 39513:697285D7-A9CA-445D-B16C-F23BF0E3B1A3

tiche79 by Associate II
  • 4205 Views
  • 11 replies
  • 0 kudos

I2C and EEprom

Posted on March 17, 2014 at 11:34Hi,I'm starting to develop an application where I'll manage EEprom data by I2C. Is there a complete example for stm32F0discovery? Thanks

mosine by Associate II
  • 1394 Views
  • 2 replies
  • 0 kudos

spi eeprom reading problem

Posted on December 13, 2012 at 00:57Hi, I am writing data into an ST 95M02SPI eeprom memory, from a STM32F051 micro but I am unable to read it back. On the scope I can see the proper data on MISO (just an incrementing count). SCK looks to be fine, (...

stenasc by Senior
  • 2804 Views
  • 6 replies
  • 0 kudos

STM32L-Discovery and PMB-648 SiRF (GPS Module)

Posted on March 21, 2014 at 04:18 Hey there. I am trying to receive TTL messages sent from my PMB-648 to my STM32L-Discovery board on pin PC11 but I'm having trouble. Whenever I debug my code it hangs on the while loop, waiting for data to arriv...

jbh0001 by Associate II
  • 1188 Views
  • 2 replies
  • 0 kudos

STM32F USB Device with USB3 host

Posted on March 12, 2014 at 17:40Hi,I'm developing both a driver on the host side and application on the client/device side using the onboard FS phy. Provided the host is USB2 both sides are behaving as expected. If I plug the device into a USB3 por...

DMA and CPU accessing SRAM same time

Posted on March 19, 2014 at 15:28Hi,I am working on a system using STM 32F107 processor(connectivity line). Because of our requirement same memory location of SRAM is accessed by both CPU and DMA. CPU is supposed to move the data from initial locati...

nmadhavan by Associate II
  • 11738 Views
  • 7 replies
  • 0 kudos

ADC regular channel not ready after enabling ADC

Posted on June 09, 2012 at 21:53I'm trying to use a single ADC channel on a STM32L151 using Keil Realview and ST libraries. After enabling the ADC I wait until the ADONS bit is set indicating the ADC is ready to convert but it does not set. Looking ...

bluscape by Associate III
  • 2253 Views
  • 6 replies
  • 0 kudos

Problem sending with USART_SendData

Posted on March 20, 2014 at 16:25 USART_SendData(USART1, 12); USART_SendData(USART1, v_dc_int); USART_SendData(USART1, v_dc_fra); If I send only one of the it is received fine. But if I send them all, I only can see the last of them. Do I...

pedroh44 by Associate
  • 1036 Views
  • 1 replies
  • 0 kudos

delay function Mcs o mls

Posted on March 18, 2014 at 22:06Hi, I'm looking how to perform a  delay function whith microsecondor milisecande Who can help me ?thank you alot

haythem by Associate II
  • 2940 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.