DELAY help
Posted on July 19, 2013 at 07:34Im trying to create a delay but im lost on how to make one, any code would be great.-Tim
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on July 19, 2013 at 07:34Im trying to create a delay but im lost on how to make one, any code would be great.-Tim
Posted on September 14, 2012 at 14:29 I'm working on a project on a STM32F4 CPU, generating signals (VGA) with DMA. I have a generic timer on CPU clock (no prescaler) on a STM32 triggering interrupts on overflow, to generate a periodic signal ...
Posted on March 17, 2014 at 16:56I'm having a problem with my usart communication between stm32f4 and hc-05 bluetooth module. I'm trying to configure the AT command of HC-05 using the stm32 board and i'm checking the response using the USB serial mo...
Posted on March 18, 2014 at 19:38Dear all, i am still in a beginner phase with stm32, and trying to output a square wave from a GPIO PORTA pin. But program loops in hardfault: > step target state: halted target halted due to single-step, current mod...
Posted on March 11, 2014 at 11:36The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 17, 2014 at 20:36Hello everyone,I am trying to make U-boot work on my STM32F4-discovery board, and I downloaded the Emcraft version which supports the STM32F429-Disco board. I have made the required modifications (I hope) but I am fa...
Posted on March 18, 2014 at 16:35 Hello all, I’ve been fighting for 2 days with a STM32F4-Discovery board to get the Timer 3 counting properly in External Counting Mode 2 but I can’t figure out what’s wrong in my code or in the MCU config. ...
Posted on January 03, 2012 at 17:08Hi All, I starting to use the STM32 with lwIP stack and I will need to use the multicast. Is there any example or demo for this ??? Thank you in advance. With Best Regards #stm32-+-lwip-+-multicast
Posted on March 18, 2014 at 13:32Problem: ST-Link utility can't connect the target MC.First of all I connected all the wires as necessarySWCLK-PA14, SWDIO-PA13, GNDand checked the quality of connections. Everything is OK.my program just configures P...
Posted on March 18, 2014 at 15:48HiI'm trying to read data from camera ov7670 with FIFO (AL422) with a stm32f4 micro controller. can I do this without using DCMI interface?if yes how can I do this? and is it necessary to use DMA?thanks #connecti...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.