2014-03-19 8:08 AM
Hello, I have a STM32F100RBT6B board, and I should use some sensors
LSM303D
with I2C
.
Just a question: wich is the maximum number of sensors that I can use with an I2C interface? #sensor #i2c2014-03-19 8:18 AM
wich is the maximum number of sensors that I can use with an I2C interface?
Will be limited by the number of unique addresses you can assign to the devices you plan on using, in the case of the part you mentioned that would be TWO, controlled by the SA0 pin2014-03-19 8:23 AM
Thanks for the answer. So if I would like to control 4 sensors, should I use both I2C interface? In this case, is it impossible to control 5 sensor?
2014-03-19 8:46 AM
So if I would like to control 4 sensors, ...
Not correct. I2C uses the LSB to differ between read and write access, so you can attach only two devices to one bus without interference. That is even described in the LSM303D datasheet (see sect. 6.1.1).
2014-03-19 9:00 AM
Thank you very much
2014-03-19 9:06 AM
Thank you very much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.