Ask questions, find answers, and share insights on STM32 products and their technical features.
Hello,I'm wondering if there's a way to use the DSIHOST_D1P and D1N pins as GPIOs, or if it's possible to simulate GPIO functionality on these pins. Currently, I don't see any GPIO configuration options for them in STM32CubeMX. The MCU in use is the ...
Using the STM32U083C-DK discovery board with STM32CubeIDE and set up the project using the Device Configuration Tool.Set up a simple program to transmit 8-bit data out one UART using interrupts and receive it in another UART using DMA.Variables used:...
I am writing my own SPI driver, and using two B-L072Z-LRWAN1 boards to test them; one as an SPI master and one as a slave. On the master device, whenever I enable the SPE bit in the function SPI_Transmit(), it never actually sets to '1', even though ...
Hi, https://community.st.com/t5/stm32-mcus-products/configuring-ppp-on-stm32f407disc-with-lte-modem-via-usart-using/m-p/728673#M262741 This continues the previous thread discussing the PPPoS implementation for the STM32F407. I successfully establishe...
Hello Everyone,Is there any plan for ST to provide support drivers for the MX25L6433F serial NOR flash on the STM32H5 series of micros?MX25L6433F is the flash used on the X-NUCLEO-GFX01M2.Thanks.
Hello STM32 Community,I’m working with a custom board featuring the STM32H725ZGT6, and I’m encountering some issues I hope you can help with. Out of the 10 boards I've assembled, 7 are functioning perfectly. However, on a few boards, the MCU isn’t be...
Greetings Sir/Mam,I have some questions about STM32 MCU Chips. Sir/Mam, I want to know if the STM32 MCU Chip Programming is possible, you may view the video on- https://www.youtube.com/watch?v=ndEeFQ5mi_g&t=106s , to get about my question. Sir/Mam, ...
Hello,I am using the SPI on the STM32H743ZITx as a SPI Master in Full-duplex mode to transfer large data packets (1600 bytes). But instead of seeing the data being transferred in a constant burst, I see it being sent out a byte at a time with gaps in...
Using STM32G0B1 device, DFU FW update is working as expectedIncluding leave request, wich results in expected device leave and start at requested addressBut `dfu-util` returns error status due to get_status error after leave requestAs stated in "AN31...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.