STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB Type-C CCx Line Configuration

Hello, I am working on Battery Management Project where I can use USB type-C. But I can use CCx line tie off with 5.1Kohm pull down resistor for 5V 3A. After this configuration USB Type-C consume 3A current at 5V.Please give me suggestion that how it...

Chintan2 by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos

LSI frequency not stable when switching power

Hello everyone,I'm working on a project using STM32U031, and using RTC with LSI(32kHz) to calculate elapsed time, and everything working fine, the waveform of LSI output also looks great.And I need to switching power supply in sometimes, and there co...

kein_1-1731487049901.png
kein by Associate III
  • 937 Views
  • 0 replies
  • 0 kudos

STM32F07- act like a dead chip.

I have a board that used STM32F07. I connect BOOT0 pin to GND via RES 10kOhm and left NRST pin open. At first i able to connect to STM32 and upload code but problem is after first time upload code (I use debug mode). It show STM is disconnect and aft...

Esa1 by Associate II
  • 988 Views
  • 1 replies
  • 0 kudos

STM32L011F4P6 can't upload code.

I have STM32L011 board that i make. I left NRST and BOOT0 open. And i try to upload code using ST Link V2. But seem like the ST link is not recognize the STM it always show "Target no device found". Can anyone help me identify the problem? Please..Th...

Esa1 by Associate II
  • 4547 Views
  • 11 replies
  • 0 kudos

STM32H7 + FMC + MDMA transmits only the first halfword

Hello everybody,Im am currently trying to connect a STM32H753 to a AD7606B using the parallel interface (FMC) and got it working at some point where the CPU can read/write the data from/to the FMC but it needs a __DSB() before starting to use the rea...

ABouk.1 by Associate III
  • 1370 Views
  • 0 replies
  • 0 kudos

Explain Output Speed STM32U575

I am working on the firmware for my STM32U575 based controller board. I cannot find in the documentation an explanation about the Low/Medium/High settings on a GPIO port. I see the bits to be set, and in MX the option for choosing the setting, but I ...

ScottD by Associate II
  • 1767 Views
  • 2 replies
  • 6 kudos

Bare Metal STM32L496

void SystemClock_Config(void) { // Step 1: Enable HSI RCC->CR |= RCC_CR_HSION; // Enable HSI while (!(RCC->CR & RCC_CR_HSIRDY)); // Wait until HSI is ready // Step 2: Configure the voltage scaling PWR->CR1 |= PWR_CR1_VOS_0; // Set voltage scale to 1...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.