STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! OCTOSPI on STM32U5F9ZJT6Q

Dear,  Can you confirm that OCTOSPI P2 is available only on WLCSP208 and TFBGA216 packages of this series?  I wanted to use both OCTOSPI interfaces in LQFP144, but noticed that there is missing only OCTOSPIM_P2_IO3 line in it, so my conclusion is tha...

Ivica by Associate
  • 2169 Views
  • 6 replies
  • 2 kudos

Resolved! (FD)CAN module resends with ACK visible on bus

Hello everybody, I am new here so please let me know, if there is important information missing. Thank you already for you time! I set up a STM32U575I-EV board for communication with CAN. The STM Board, a PCAN-USB dongle and an Oszilloskope are conne...

Oszi_ACK.png
finally by Associate II
  • 333 Views
  • 4 replies
  • 1 kudos

Resolved! Feature request: Programmable logic

I am a fan of STM32, especially the peripheral sets offered are great. Over the years however, one type of peripheral is missing which would be a great help for many projects, this is a programmable logic cell.Such a cell would contain elements like ...

LVan .31 by Associate III
  • 13684 Views
  • 35 replies
  • 25 kudos

Resolved! Please clarify IO state in standby mode

I would like to refer you to the following post from @JRuss.4 that was never satisfactorily answered:STM32L4 Standby Mode GPIO State {Schmitt Trigger} Clarification from Reference Manual I also have the exact same question.   Here is my version of th...

AMacd.1 by Senior
  • 346 Views
  • 3 replies
  • 1 kudos

STM32H757: TDM slots and bit depth over SAI interface

I'm working on a device that requires requires 12 audio output channels and 10 input channels. I wish to do this over 16-slot TDM. Now, I'm concerned about whether this can be done with 32 bits per sample. The reference manual states in section 54.4....

Zipper by Associate II
  • 345 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G474 HRTIMER Deadtime on skipped pulse.

I've STM32G474 using the HRTIMER to control a boost converter, each channel has it's own converter. This all works nicely with the deadtime, no issues. When I come to do a pulse skip, (set CMP3 to 0) the deadtime is still being inserted in the the Tx...

Resolved! How to find out SPI controller version

Hi,I would like to know where I can find the SPI controller version of the STM32G491.AN5543 lists features depending on the SPI controller version and says "To identify the version and the available feature set refer to the product reference manual a...

seb234 by Associate
  • 242 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.