STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to identify information printed on STM32F407IGT6 chips?

I have two STM32F407IGT6 chips, and I need help understanding the markings printed on their surfaces.Images attached:First chip: "STM32F407IGT6 AA295 VQ 6 TWN AA 342"Second chip: "STM32F407IGT6 VQ249473 AA297 TWN AA 318"I would like to know:What each...

Muk_0-1732272258299.png Muk_1-1732272261127.png
Muk by Associate II
  • 2929 Views
  • 4 replies
  • 1 kudos

Timer/Usart priority problem

While testing the Blackpill Timers and Usarts I came across this problem. If I set for example 6 timer channels using two timers. (In my case Tim2 and Tim3 and Usart1. If I set all six channels to PWM generation, I find it difficult to dynamically re...

techdesk by Associate III
  • 2274 Views
  • 4 replies
  • 0 kudos

Resolved! Pushbutton causing multiple ISR flags (EXT-> PR) to set??

So I have three switches (nothing special just momentary push button) wired into the board PC2, PC3 and PA4. All are using internal pullups. PC2 and PC3 are set for rising / falling trigger IRQs and PA4 is set for falling IRQ. They all have their own...

SWenn1_0-1732482589937.png
SWenn.1 by Senior III
  • 4687 Views
  • 10 replies
  • 0 kudos

Odd Behavior of TIM2 PWM Output on STM32U073

In a system using FreeRTOS, there are currently two timers: TIM6 (the timer used by FreeRTOS) and TIM3 (a general-purpose timer). I am not experiencing any issues with these timers, and I can successfully run functions like interrupts. However, whene...

muratsimsek_0-1732537382675.png

STM32H7A FMC Common and Attribute Memory Space

Hello. I am working on a project where I need to access an external Flash chip on a STM32H7A3ZIT6 chip. I am trying to use the FMC and I'm just having a hard time understanding it. My biggest lack of understanding is coming in how in the world do I p...

FMC_common_attribute_split.png Screenshot 2024-11-23 162458.png
L42Liam by Associate
  • 1441 Views
  • 1 replies
  • 0 kudos

Resolved! Maximum supported resolution for the STM32U5G9?

Hello, I would like to know what is the maximum display resolution that can be supported by the STM32U5G9 chip, I calculated based on the MIPI clock that I can drive a 1024x768 screen at 16 bit, but I am very unsure. Thanks for your help.

Smith_023 by Associate II
  • 2874 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.