2024-11-25 4:24 AM - last edited on 2024-11-25 7:36 AM by mƎALLEm
In a system using FreeRTOS, there are currently two timers: TIM6 (the timer used by FreeRTOS) and TIM3 (a general-purpose timer). I am not experiencing any issues with these timers, and I can successfully run functions like interrupts. However, whenever I try to generate a PWM output using TIM7, I have not been able to achieve it.
Here is the main code.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
MX_CRC_Init();
MX_DAC1_Init();
MX_TIM3_Init();
MX_USART2_UART_Init();
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1); <---- STARTING PWM
/* USER CODE END 2 */
/* Init scheduler */
osKernelInitialize();
/* Call init function for freertos objects (in cmsis_os2.c) */
MX_FREERTOS_Init();
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2024-11-25 6:51 AM
Hello,
@muratsimsek wrote:
However, whenever I try to generate a PWM output using TIM7, I have not been able to achieve it.
But in the code, nothing about TIM7 but only TIM2:
MX_TIM2_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1); <---- STARTING PWM
2024-11-25 6:53 AM
And your title: "Odd Behavior of TIM2 PWM Output on STM32U073" -> confusing information!
Need to clarify and fix.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.