2014-12-11 11:53 PM
I am migrating code from STM3210x to STM32F0xx. major part of the application uses spi interface. I see in logic analyzer each bursts of 16bit clocks. while I expect it to be 8bit clock for each byte and a delay of one byte between the clocks. I am attaching the signals.
inside attachments you can so how its initialized and the outcome. Can someone suggest how to get the same signaling in STM32F0 to be like the STM32F10 ?I have tried using SPI_Senddata8, change the SPI_InitStructure.SPI_DataSize with no success.The code I am using is as folow: SPIx_CS_GPIO->BRR = SPIx_CS; for(i=0; i<headerLength; i++) { SPIx->DR = headerBuffer[i]; while((SPIx->SR & SPI_I2S_FLAG_RXNE) == (uint16_t)RESET); temp = SPIx->DR ; } for(i=0; i<readlength; i++) { SPIx->DR = 0; while((SPIx->SR & SPI_I2S_FLAG_RXNE) == (uint16_t)RESET); readBuffer[i] = SPIx->DR ;//port_SPIx_receive_data(); //this clears RXNE bit } SPIx_CS_GPIO->BSRR = SPIx_CS;Thanks,Roy #stm32f0We’re moving the ST Community to a new platform to give you a better and more reliable community experience.