2014-12-11 11:57 PM
Hello forum,
I have a weird issue with TIM's pending bits (I mean Cortex-M3 pending bits): they are set after enabling the overflow interrupt: void InitTIM4() { TIM_TimeBaseInitTypeDef timer; TIM_TimeBaseStructInit(&timer); timer.TIM_CounterMode = TIM_CounterMode_Up; timer.TIM_Prescaler = 9; timer.TIM_Period = 79; TIM_TimeBaseInit(TIM4, &timer); TIM_Cmd(TIM4, ENABLE); TIM_ITConfig(TIM4, TIM_IT_Update, ENABLE); } Therefore after enabling all interrupts with __enable_irq (), program goes to corresponding Handlers immediately, although it should go there after TIM overflows. I tried clearing pending bits with NVIC_ClearPendingIRQ() but it didn't work. Maybe i'm not understanding or missing something simple, i don't know. I'm using STM32F100RB MCU. Sorry for my poor English.2014-12-12 2:30 AM
Nevermind. I didnt clear request interrupt AND pending interrupt after the TIM4->EGR |= TIM_EGR_UG
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.