STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 CAN Transmit doesn't work

Posted on December 15, 2014 at 17:13 Hello! I use STM32F407 Discovery board and want to use CAN1. My IDE is CoocoxIDE. I've putoscilloscopeon line PD1 (CAN TX) and haven't seen any activity...Discovery CAN works without any CAN IC (CAN Driver...

vasyl by Associate
  • 1033 Views
  • 1 replies
  • 0 kudos

EXTI Problem with nucleo L152

Posted on December 14, 2014 at 14:21Hello,I've got a strange problem with setting an interrupt for input pins on my Nucleo board. Actualy, no one interrupt except EXTI15_10_IRQn doesn't work. I'm attaching two portions of code, one using input pin 1...

leosad by Associate II
  • 1947 Views
  • 3 replies
  • 0 kudos

DMA to external DAC transfer via SPI communication

Posted on November 13, 2014 at 13:32Hi everybody, I'm a beginner with STM32F30x µP. I'd like to made a DMA transfers from SRAM to an external DAC via SPI communication. Is it possible? Can I even configure a timer (TIMx) to generate a PWM signal or ...

franck2 by Associate II
  • 4365 Views
  • 19 replies
  • 0 kudos

no ir camera with stm32f4 discovery

Posted on December 15, 2014 at 00:08I want to use an infrared camera with stm32f4 discovery board. I thought in use a no ir raspberry pi camera, but I couldn't find any datasheet and pinout from this camera. Anyone know if I can use this camera with...

stm32nucleo legacy firmware

Posted on December 14, 2014 at 03:49Hi,I want to know where I can get the legacy libraries for stm32f401 nucleo boards (STM32 Nucleo_FW_VX.Y.Z) because I dont want to work with cube libraries.

gevides by Associate II
  • 1211 Views
  • 1 replies
  • 0 kudos

STM32Cube USB Host : device disconnection not detected !

Posted on December 10, 2014 at 19:10Hello ! I'm trying to write a MIDIstreaming class host driver based on the CDC example. First detection of the device and class initialisation work at boot and after boot. But the disconnection and reconnection of...

bluexav by Associate III
  • 1294 Views
  • 1 replies
  • 0 kudos

STM32F0 WITH Assembly

Posted on November 30, 2014 at 13:00 Dear All , I written a program in assembly to tern on bit 8 on GPOIC It is compiled well but LED does not on processor STM32F051R8T6 IDE KEIL PRESERVE8 THUMB RCC_APB2ENR EQU 0X40021018 ...

pic_micro by Associate II
  • 8963 Views
  • 39 replies
  • 0 kudos

Interrupt problem and UART problem

Posted on December 05, 2014 at 03:03Hi ST forum,I have two separate problems: 1. How do I configure an interrupt to do X on rising edge and Y on falling edge? Currently, I can only do rising edge: (Solved, see below)/********************************...

STM32F042K6 Not always starting code execution

Posted on December 11, 2014 at 20:07Setup: I used CubeMX to generate and added code to blink 2 leds and compiled with IAR Embedded. LEDs are connected to PB3 and PB5. I have several boards I soldered 042's to with proper caps, and leds with current ...

dan by Associate II
  • 4051 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.