STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding GPIO Feature

Posted on November 23, 2014 at 14:05Hi, Ive been using several MCU before. Its my first time to use STMicro.Now Im currently studying its architecture.My question is, what is the use of GPIO BSRR (Bit Set Reset Register) when we can access or write ...

USART2 Switching TX and RX Pins

Posted on August 17, 2015 at 22:32Hi,I am currently working with an STMF103RB on a board I made. I am using the STMCube_FW_F1_V1.2.0 libraries. I am currently using USART2 to connect to a computer though an FTDI breakout board. Everything works fine...

sacraig by Associate II
  • 2616 Views
  • 4 replies
  • 0 kudos

STM32F10x StdPeriph SPI DMA ?

Posted on August 16, 2015 at 11:16Guys, I want  to try the example from : STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\SPI\DMA and I follow from readme.txt par How to use it ? In order to make the program work, you must do th...

Interfacing a CIS with STM32F

Posted on August 16, 2015 at 23:54Hello everyone,I have a project in which I am using a Contact Image Sensor. I receive an analog signal at 4 MHz which represents the color of a pixel. I have to transform it into a digital signal of 8 bits ( this re...

ed_62 by Associate II
  • 3401 Views
  • 5 replies
  • 0 kudos

System crash with all core registers value as 0xFFFFFFFF

Posted on August 17, 2015 at 08:59I have a system(freeRTOS) running well on stm32f401 platform. To reduce the PowerConsumption, i added a HAL_PWR_EnterSLEEPMode() into the void vApplicationIdleHook( void ). The system will crash in seconds with all ...

bzhang by Associate
  • 638 Views
  • 1 replies
  • 0 kudos

STM32F407 - Multi-ADC mode with DMA

Posted on January 09, 2014 at 15:19How is the DMA supposed to work with Triple-ADC Regulare mode? The documentation shows an ADC stream for each ADC, but it also seems to indicate that it will be working with a single DMA stream for this process. ...

dibs by Associate II
  • 4277 Views
  • 10 replies
  • 0 kudos

STM32Cube F4 USB CDC Rx only once!

Posted on August 14, 2015 at 09:54HW board is stm32f429I-Discovery (MCU: stm32f429ZIT6).I use STM32Cube MX V4.9 and stm32f429 firmware package V1.7 to generate source code of USB CDC function. GUI select device_only mode, and HSE to external 8MHz cr...

tristan by Associate
  • 1083 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.