STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Forum participation by ST

Posted on October 01, 2012 at 16:10Would it be possible for ST, it's technical staff, or FAE's to participate in this forum in a more meaningful way? #evertdekker.com

STM32F4 DISCO and CS43L22 DAC

Posted on August 11, 2015 at 07:59Hey everybody :) The STM32F4 disco has an external audio DAC witch is still a little hard to grasp for me, I was hoping anybody of You know any good tutorials, where it would explain how to get a sampling frequency ...

matas by Associate II
  • 1425 Views
  • 3 replies
  • 0 kudos

GPIO_analog vs ADC, STM32F2

Posted on August 16, 2015 at 09:401. Microxplorer gives option to set any GPIO pin as GPIO_analog or pin as ADC if it has ADC feature.2. What is diff between two. I know abt ADC but what does GPIO_analog do?

STM32L0 in UFQFPN32 with HSE

Posted on August 15, 2015 at 11:08Hi, I am looking for an STM32 which has:- A 5x5 mm package which can be used on a 2 layer board (that excludes BGA, I suppose)- 32 or more pins- Ultra low power- DAC- Crystal main clockIn the parametric selection, t...

soren by Associate II
  • 1527 Views
  • 2 replies
  • 0 kudos

STM32F7 discovery kit problem with QSPI

Posted on August 15, 2015 at 10:41Hello, I'm using the STM32F7 discovery kit from ST with Keil uV5, the kit is great however I tried to reload the demonstration firmware, Keil always reports that ''no algorithm found for: <all address in QSPI memory...

Pin termination normally & after power up STM32

Posted on August 14, 2015 at 12:22I am using STM32F205 LQFP64 & want to know if below configuration of pin are ok. I use SWD method.I have grouped pins as:1. vbat:  If not used, connect it to Vdd & decouple by 0.1uf cap.2. PA0-PA15: If any of pin is...

window watchdog example for stm32f103

Posted on August 15, 2015 at 09:59hi every one. i am trying to initial wwdg of stm32f103rbt6 & i am using cmsis libraries for this. based on cmsis examples i wrote my program & it compiled succesfully but dose not work correctly. i attached example,...

mhdizgah by Associate II
  • 1345 Views
  • 1 replies
  • 0 kudos

STM32VLDISCOVERY Keil Assembly Project from Scratch

Posted on June 28, 2013 at 05:44I require to build an assembly project in the STM32VLDISCOVERY board either using Keil's  startup file (startup_stm32f10x_md_vl.s) or no startup file at all. The project must have either absolute (preferably) or reloc...

fj by Associate
  • 4044 Views
  • 7 replies
  • 0 kudos

Software trigged DMA!

Posted on August 15, 2015 at 08:09 STM32F103C8 What is the proper setup of a software trigged DMA? Or how do one setup TIM4 so software trigger DMA works? I get a conflict between TIM4 CCR1 match triggered DMA (which works pe...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.