STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! JTAG signals on STM32L433 [RESOLVED]

Hello,for the project I am developing I am using a STM32L433.We have connected a motor encoder signals to PA15 and PB3, that are CH1 and CH2 for timer1 TIM2 configured in encoder mode.We used CubeMX to configure the HW, and that worked perfectly for ...

MauroF by Associate II
  • 2942 Views
  • 6 replies
  • 2 kudos

I3C TxFIFO target limit

Hello, I am working with the STM32H503 board and using the I3C TX FIFO in target mode for communication. However, I have encountered an issue where, when transmitting data, the FIFO is only sending 8 bytes in total. I would like to configure the TX F...

Resolved! documentation error AN4777

In the first page of AN4777, the RM0411 is listed as the reference document for STM32L4x6. There is no link to the document and i am unable to found it. Also in STM32L4x6 page, the reference manual is named RM0351 instead of RM0411.

nicolas by Senior II
  • 1881 Views
  • 2 replies
  • 1 kudos

nucleo-F756ZG with Qorvo DWM3000

Hello,I have connected the nucleo f756zg board with the qorvo dwm3000. I found the inc and src files for the dwm3000 but the drivers for the dwm3000 are available for the m33 and m4 families.Is it someone who used an M7-Cortex mcu and have the driver...

Resolved! STM32H723 DACs

The datasheet for STM32H723VG (https://www.st.com/en/microcontrollers-microprocessors/stm32h723vg.html) states that the devices have 2 x 12 bit, 2-channel DACs. However, in STM32CubeMX I see only one DAC listed (device = STM32H723VGT6).Is this an err...

Repwoc_1-1733832699606.png Repwoc_0-1733832663426.png
Repwoc by Associate III
  • 2538 Views
  • 5 replies
  • 1 kudos

Heap size for STM32F101RG

Hello,I have a question on how to optimally configure the RAM of the STM32F101RG.The controller has 1MByte Flash, 80KByte RAM. I need to use most RAM for Heapsize and I configured within Keil IDE under target options/ASM0xCD00 for Heap size and0x1000...

KauneR by Associate III
  • 1549 Views
  • 2 replies
  • 0 kudos

I2C Timing Configration

Hi, Please tell me about I2C timing configration. I use Nucleo-L552ZE-Q. I set up the I2C as shown in the picture following the reference manual(RM0438, Table 326). The fi2cclk is 48MHz.   But SCL cycle is very slow.  How can I set the SCL cycle to...

115840.jpg 115937.jpg
DK3 by Associate II
  • 1314 Views
  • 2 replies
  • 0 kudos

Resolved! FDCAN no ACK

Hi,I am trying to use a STM32G491KEU6 with FDCAN, but the communication is failing at line:if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxData) != HAL_OK) { ...I found out that this is a problem that receiver is not sending a ACK bit - cann...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.