STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Blink program not working

Posted on September 19, 2015 at 17:55Hi to all, I am trying to write my first program for STM32F0 discovery board. Of course the first step is to make a LED blink, but, till now, I failed. I created the program using CubeMX and of course it worked. ...

STM32F4 FSMC interfacing with SDRAM

Posted on October 03, 2013 at 05:35Hi,I kwow STM32F4 support FSMC interface with LCD, FLASH...and SRAM/SDRAM...I have some example FSMC with LCD, SRAM but I don't kwow how to interface and control SDRAM. Can anyone show me an example (schematic, pri...

STM32_F103VE RCC_CR write issue

Posted on October 17, 2015 at 11:05I am working on a project using internal clock though PLL as system clock,here is the issue:1.HSI is 8MHz.2.System is programmed to wake and sleep in 1 second period (Stop mode, using WFI), which is waked by RTC al...

CubeMX Race condition

Posted on October 19, 2015 at 00:11The generated code initializes all peripherals and enables interrupts.The application code's first hook is after peripheral initialization.How do I ensure that no interrupts before all high level peripherals are re...

osama2 by Associate II
  • 643 Views
  • 0 replies
  • 0 kudos

STM32Cube Feature Request - USB Composite Device

Posted on October 17, 2015 at 16:57Hello ST,I'd like to suggest to add the feature of USB composite devices (e.g. CDC + HID - or 2 times CDC). This would improve the STM32Cube's usefulness a LOT!Until that feature is implemented:Can anyone give me a...

dpfeffer9 by Associate II
  • 1037 Views
  • 1 replies
  • 0 kudos

DMA events like functionality

Posted on October 18, 2015 at 19:57Hello there,I know that dma can be used to transfer data from/to peripherals to memory and etc. I was wondering though would it be possible to use the dma for registering certain events instead of interrupts?For ex...

emc problem about radiation emission on GPIO at PUSH-PULL mode

Posted on October 17, 2015 at 03:40I use STM32F373, freq of PLL is 72MHz.If one pin (PD1, PD2 or any pin) is configured in PUSH-PULL mode, then 144MHz harmonic is immediately detected at this pin by the near field probe with one spectrum analyzer.If...

yundm2 by Associate II
  • 1820 Views
  • 2 replies
  • 0 kudos

st-link error

Posted on February 05, 2013 at 06:41I am using stm32-f407 discovery board with IAR. It was working quite fine but when i tried to interface a 16 x 2 lcd and downloaded the code, it gave the following error .  Fatal error: ST-Link, No MCU device foun...

Want to trigger DMA from Timer

Posted on October 14, 2015 at 18:22 I am using the ST32f I would like TIM4 to trigger the DMA which should move data from memory to SPI2. Tim4 count is changing but it does not trigger the DMA. Can somebody please point out where I am go...

JustMe by Associate III
  • 3066 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.