STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F207 DMA ADC Read with pin state change

Posted on October 19, 2015 at 17:02Hi, is it possible to have the pin state changed during ADC DMA Regular Simultaneous mode so that the pin that has been read is set to OUTPUT LOW while the one that is read is INPUT?The current otherwise leaks thro...

STM Studio - STM32 PMSM FOC LIBv4.2 - Speed Variable

Posted on October 19, 2015 at 13:36Hi, I am running the STM32 PMSM FOC LIBv4.2, using encoder and I am trying to visualize the variables values through the STM Studio. The variable names used here are the default used in the STM32 PMSM FOC LIBv4.2I ...

cviolino by Associate II
  • 1102 Views
  • 1 replies
  • 0 kudos

STM32f427 - SPI with DMA problem (HardFault)

Posted on October 19, 2015 at 10:53 Hello all, I work with a STM32F427 and the HAL libraries, and i want tu use the SPI with DMA. Configuration : The chip is in slave mode and receive datas from an ADC converter. The Clock and NS...

astier by Associate
  • 2065 Views
  • 2 replies
  • 0 kudos

debugging in STOP mode

Posted on January 07, 2014 at 17:37 I develop a lot of low power applications using STM32 and I'd like the ability to use the debugger while in low power STOP mode. My code works as expected in release mode (i.e. no debugger) but when debugging ...

trevor23 by Associate III
  • 8280 Views
  • 9 replies
  • 0 kudos

STM32F407 Enable Can Error Irq

Posted on October 16, 2015 at 17:19Hello, I would like to enable the CAN error Irq and in particular the LEC so in my init function I did CAN_ITConfig( CAN2, CAN_IT_TME | CAN_IT_FMP0 | CAN_IT_FOV0 | CAN_IT_FF0 | CAN_IT_LEC | CAN_IT_ERR, ENABLE ); an...

STM32L15xxC Vcore Range 3 must not be used

Posted on October 19, 2015 at 14:25Hi all, Having a look at the Errata sheet for STM32L100RC and STM32L15xxC (DocID025807 Rev 4) I could read in point 2.1.4 Range 3 of dynamic voltage scaling cannot be used. In fact, in further detail description s...

guillem2 by Associate II
  • 547 Views
  • 0 replies
  • 0 kudos

low transfer rate when using USB MSD device based on STM Cube

Posted on October 19, 2015 at 10:10Hi,I am using the STM Cube framework to implement a USB Mass storage device supporting high speed USB for my STM32L151 device. When transferring files from the device to a Windows 8 laptop, I consistently see a tra...

bnp979 by Associate III
  • 1179 Views
  • 1 replies
  • 0 kudos

STM32F407 GPIO not toggles on 168MHz SysClk

Posted on October 16, 2015 at 11:31Good day, I use CooCox 1.7.8 and STM32F4DISCOVERY as programmator. Problem is, that after re-configuring SysClk to PLL running on 168MHz (which is confirmed through observing 84MHz on MCO1 output) ToggleBit comma...

kvg by Associate II
  • 1718 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.