2015-10-18 3:11 PM
The generated code initializes all peripherals and enables interrupts.
The application code's first hook is after peripheral initialization.How do I ensure that no interrupts before all high level peripherals are ready?Example:In the RTC IRQ handler I read data from a sensor.The sensor needs an initialization sequence before being operational.Too bad that the RTC interrupt is enabled *before* I can initialize the sensor.RTC-Interrupt orrurs, sensor not yet ready, crash.__disable_irq() / __enable_irq() is not an option because it blocks SysTick which the initialization code relies on.Off Course I can do ''IfSensorIsEnabled()'' in the RTC IRQ handler but why should I?IMHO this is another case of bad embedded software architecture in CubeMX./OsamaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.